Store group table entries in RAM or in tokens, depending on the platform. If the endpoint field is SL_ZIGBEE_AF_GROUP_TABLE_UNUSED_ENDPOINT_ID, the entry is unused.
Public Attribute Documentation#
endpoint#
uint8_t sl_zigbee_af_group_table_entry_t::endpoint
Definition at line
964
of file app/framework/include/af-types.h
groupId#
uint16_t sl_zigbee_af_group_table_entry_t::groupId
Definition at line
965
of file app/framework/include/af-types.h
bindingIndex#
uint8_t sl_zigbee_af_group_table_entry_t::bindingIndex
Definition at line
966
of file app/framework/include/af-types.h