Describe a load control event.
This struct is used in the load control event callback and within the demand response load control cluster code.
Public Attributes#
uint32_t
uint8_t
uint16_t
uint8_t
uint32_t
uint16_t
uint8_t
uint8_t
uint8_t
int16_t
int16_t
int8_t
uint8_t
uint8_t
uint32_t
uint32_t
uint8_t
Public Attribute Documentation#
eventId#
uint32_t sl_zigbee_af_load_control_event_t::eventId
Definition at line
632
of file app/framework/include/af-types.h
destinationEndpoint#
uint8_t sl_zigbee_af_load_control_event_t::destinationEndpoint
Definition at line
642
of file app/framework/include/af-types.h
deviceClass#
uint16_t sl_zigbee_af_load_control_event_t::deviceClass
Definition at line
643
of file app/framework/include/af-types.h
utilityEnrollmentGroup#
uint8_t sl_zigbee_af_load_control_event_t::utilityEnrollmentGroup
Definition at line
644
of file app/framework/include/af-types.h
startTime#
uint32_t sl_zigbee_af_load_control_event_t::startTime
Start time in seconds
Definition at line
648
of file app/framework/include/af-types.h
duration#
uint16_t sl_zigbee_af_load_control_event_t::duration
Duration in minutes
Definition at line
652
of file app/framework/include/af-types.h
criticalityLevel#
uint8_t sl_zigbee_af_load_control_event_t::criticalityLevel
Definition at line
653
of file app/framework/include/af-types.h
coolingTempOffset#
uint8_t sl_zigbee_af_load_control_event_t::coolingTempOffset
Definition at line
654
of file app/framework/include/af-types.h
heatingTempOffset#
uint8_t sl_zigbee_af_load_control_event_t::heatingTempOffset
Definition at line
655
of file app/framework/include/af-types.h
coolingTempSetPoint#
int16_t sl_zigbee_af_load_control_event_t::coolingTempSetPoint
Definition at line
656
of file app/framework/include/af-types.h
heatingTempSetPoint#
int16_t sl_zigbee_af_load_control_event_t::heatingTempSetPoint
Definition at line
657
of file app/framework/include/af-types.h
avgLoadPercentage#
int8_t sl_zigbee_af_load_control_event_t::avgLoadPercentage
Definition at line
658
of file app/framework/include/af-types.h
dutyCycle#
uint8_t sl_zigbee_af_load_control_event_t::dutyCycle
Definition at line
659
of file app/framework/include/af-types.h
eventControl#
uint8_t sl_zigbee_af_load_control_event_t::eventControl
Definition at line
660
of file app/framework/include/af-types.h
startRand#
uint32_t sl_zigbee_af_load_control_event_t::startRand
Definition at line
661
of file app/framework/include/af-types.h
durationRand#
uint32_t sl_zigbee_af_load_control_event_t::durationRand
Definition at line
662
of file app/framework/include/af-types.h
optionControl#
uint8_t sl_zigbee_af_load_control_event_t::optionControl
Definition at line
663
of file app/framework/include/af-types.h