Public Attribute Documentation#

valid#

bool sl_zigbee_af_plugin_messaging_client_message_t::valid

Definition at line 1070 of file app/framework/include/af-types.h

active#

bool sl_zigbee_af_plugin_messaging_client_message_t::active

Definition at line 1071 of file app/framework/include/af-types.h

esiBitmask#

sl_zigbee_af_plugin_esi_management_bitmask_t sl_zigbee_af_plugin_messaging_client_message_t::esiBitmask

Definition at line 1072 of file app/framework/include/af-types.h

clientEndpoint#

uint8_t sl_zigbee_af_plugin_messaging_client_message_t::clientEndpoint

Definition at line 1073 of file app/framework/include/af-types.h

messageId#

uint32_t sl_zigbee_af_plugin_messaging_client_message_t::messageId

Definition at line 1074 of file app/framework/include/af-types.h

messageControl#

uint8_t sl_zigbee_af_plugin_messaging_client_message_t::messageControl

Definition at line 1075 of file app/framework/include/af-types.h

startTime#

uint32_t sl_zigbee_af_plugin_messaging_client_message_t::startTime

Definition at line 1076 of file app/framework/include/af-types.h

endTime#

uint32_t sl_zigbee_af_plugin_messaging_client_message_t::endTime

Definition at line 1077 of file app/framework/include/af-types.h

durationInMinutes#

uint16_t sl_zigbee_af_plugin_messaging_client_message_t::durationInMinutes

Definition at line 1078 of file app/framework/include/af-types.h

message#

uint8_t sl_zigbee_af_plugin_messaging_client_message_t::message[SL_ZIGBEE_AF_PLUGIN_MESSAGING_CLIENT_MESSAGE_SIZE+1]

Definition at line 1079 of file app/framework/include/af-types.h