Describe clusters that are on the endpoint.
Public Attribute Documentation#
cluster#
sl_zigbee_af_cluster_t* sl_zigbee_af_endpoint_type_t::cluster
Pointer to the cluster structs, describing clusters on this endpoint type.
Definition at line
502
of file app/framework/include/af-types.h
clusterCount#
uint8_t sl_zigbee_af_endpoint_type_t::clusterCount
Number of clusters in this endpoint type.
Definition at line
506
of file app/framework/include/af-types.h
endpointSize#
uint16_t sl_zigbee_af_endpoint_type_t::endpointSize
Size of all non-external, non-singlet attribute, in this endpoint type.
Definition at line
510
of file app/framework/include/af-types.h