Public Attributes#

uint32_t
uint8_t
uint32_t

Public Attribute Documentation#

providerId#

uint32_t sl_zigbee_af_device_management_tenancy_t::providerId

Definition at line 1789 of file app/framework/include/af-types.h

issuerEventId#

uint32_t sl_zigbee_af_device_management_tenancy_t::issuerEventId

Definition at line 1790 of file app/framework/include/af-types.h

tariffType#

uint8_t sl_zigbee_af_device_management_tenancy_t::tariffType

Definition at line 1791 of file app/framework/include/af-types.h

implementationDateTime#

uint32_t sl_zigbee_af_device_management_tenancy_t::implementationDateTime

Definition at line 1794 of file app/framework/include/af-types.h

tenancy#

uint32_t sl_zigbee_af_device_management_tenancy_t::tenancy

Definition at line 1795 of file app/framework/include/af-types.h