Public Attributes#

uint16_t
uint16_t

Public Attribute Documentation#

uncontrolledFlowThreshold#

uint16_t sl_zigbee_af_device_management_uncontrolled_flow_threshold_t::uncontrolledFlowThreshold

Definition at line 1833 of file app/framework/include/af-types.h

multiplier#

uint16_t sl_zigbee_af_device_management_uncontrolled_flow_threshold_t::multiplier

Definition at line 1834 of file app/framework/include/af-types.h

divisor#

uint16_t sl_zigbee_af_device_management_uncontrolled_flow_threshold_t::divisor

Definition at line 1835 of file app/framework/include/af-types.h

measurementPeriod#

uint16_t sl_zigbee_af_device_management_uncontrolled_flow_threshold_t::measurementPeriod

Definition at line 1836 of file app/framework/include/af-types.h

unitOfMeasure#

uint8_t sl_zigbee_af_device_management_uncontrolled_flow_threshold_t::unitOfMeasure

Definition at line 1837 of file app/framework/include/af-types.h

stabilisationPeriod#

uint8_t sl_zigbee_af_device_management_uncontrolled_flow_threshold_t::stabilisationPeriod

Definition at line 1838 of file app/framework/include/af-types.h