Enumerations

Description

Enumerations with stable binary representation.

Silicon Labs libraries do not use enumerations because the ARM EABI leaves their size ambiguous, which causes problems if the application is built with different flags than the library. Instead, uint8_t typedefs are used in compiled code for all enumerations. For documentation purposes, this is converted to an actual enumeration in documentation.

Macros

#define SL_ENUM (name)   enum name
Enumeration mapped to uint8_t.
#define SL_ENUM_GENERIC (name, type)   enum name
Enumeration mapped to arbitrary type.

Macro Definition Documentation

◆ SL_ENUM

#define SL_ENUM ( name ) enum name

Enumeration mapped to uint8_t.

◆ SL_ENUM_GENERIC

#define SL_ENUM_GENERIC ( name,
type
) enum name

Enumeration mapped to arbitrary type.