sl_se_command_context_t Struct Reference

SE mailbox command context.

#include <sl_se_manager_types.h>

Data Fields

SE_Command_t command
SE mailbox command struct.
bool yield
If true, yield the CPU core while waiting for the SE mailbox command to complete.

SE mailbox command context.

This structure defines the common SE mailbox command context used for all SE Manager API functions that execute SE mailbox commands. The members of this context structure should be considered internal to the SE Manager and should not be read or written directly by the user application. For members that are relevant for the user, the user can access them via corresponding set and get API functions, e.g. sl_se_set_yield() .

Field Documentation

◆ command

SE_Command_t sl_se_command_context_t::command

SE mailbox command struct.

◆ yield

bool sl_se_command_context_t::yield

If true, yield the CPU core while waiting for the SE mailbox command to complete.

If false, busy-wait, by polling the SE mailbox response register.