LFXO Initialization

Description

Initialize the LFXO oscillator.

Configure the low frequency crystal oscillator using settings in the configuration header sl_device_init_lfxo_config.h .

The precision of the oscillator can be indicated using the configuration option SL_DEVICE_INIT_LFXO_PRECISION . This is used by certain wireless stacks to optimize wakeup time for scheduled events (such as Bluetooth advertising).

Functions

sl_status_t sl_device_init_lfxo (void)
Initialize LFXO.

Function Documentation

◆ sl_device_init_lfxo()

sl_status_t sl_device_init_lfxo ( void )

Initialize LFXO.

Configure the low frequency crystal oscillator using settings in the configuration header sl_device_init_lfxo_config.h .

The precision of the oscillator can be indicated using the configuration option SL_DEVICE_INIT_LFXO_PRECISION . This is used by certain wireless stacks to optimize wakeup time for scheduled events (such as Bluetooth advertising).

Returns
Status code
Return values
SL_STATUS_OK LFXO initialized successfully