SensorStruct_t Struct Reference

Stores all runtime values for an enabled capacitive sensor.

#include <cslib.h>

Data Fields

uint32_t rawBuffer [ DEF_SENSOR_BUFFER_SIZE ]
Newest sample taken from CS hardware, without any processing.
uint32_t currentBaseline
Runtime estimate of untouched or inactive state of CS sensor input.
uint8_t touchDeltaDiv16
Describes the expected difference between untouched and touched CS value.
uint8_t activeIndicator
Bit array showing whether touch is qualified on sensor, uses DEBOUNCE_ACTIVE_MASK.
uint8_t debounceCounts
Stores consecutive CS values above or below active or inactive threshold.
signed char baselineAccumulator
Tracks trend of CS values to determine whether baseline rises or falls.
SI_UU32_t expValue
Filtered CS value with 16 bits of LSBs.

Stores all runtime values for an enabled capacitive sensor.

Field Documentation

◆ rawBuffer

uint32_t SensorStruct_t::rawBuffer[ DEF_SENSOR_BUFFER_SIZE ]

Newest sample taken from CS hardware, without any processing.

◆ currentBaseline

uint32_t SensorStruct_t::currentBaseline

Runtime estimate of untouched or inactive state of CS sensor input.

◆ touchDeltaDiv16

uint8_t SensorStruct_t::touchDeltaDiv16

Describes the expected difference between untouched and touched CS value.

◆ activeIndicator

uint8_t SensorStruct_t::activeIndicator

Bit array showing whether touch is qualified on sensor, uses DEBOUNCE_ACTIVE_MASK.

◆ debounceCounts

uint8_t SensorStruct_t::debounceCounts

Stores consecutive CS values above or below active or inactive threshold.

◆ baselineAccumulator

signed char SensorStruct_t::baselineAccumulator

Tracks trend of CS values to determine whether baseline rises or falls.

◆ expValue

SI_UU32_t SensorStruct_t::expValue

Filtered CS value with 16 bits of LSBs.