COMMON - Common Utilities
Description
General purpose utilities and cross-compiler support.
This SDK supports the following compilers/IDEs:
- Simplicity Studio
- IAR Embedded Workbench
- Keil µVision IDE
- Plain armgcc
Certain compiler features such as alignment is implemented differently in the tools. Therefore, macros such as SL_ALIGN are provided to enable compiler independent code.
- Note
- RAM code macros are implemented in a separate module RAMFUNC - RAM Function Support. Cross-compiler RAM code support needs extended documentation and it is therefore implemented as a separate module.
Functions | |
uint32_t | SL_CTZ (uint32_t value) |
Count trailing number of zeros. | |
uint32_t | SL_RBIT (uint32_t value) |
Reverse the bits. | |
uint32_t | SL_RBIT16 (uint32_t value) |
Reverse the bits. | |
uint32_t | SL_Log2ToDiv (uint32_t log2) |
Convert logarithm of 2 to division factor. | |
Macros | |
#define | SL_CEILING(n, i) ((((n) + (i) - 1U) / (i)) * (i)) |
Round n up to closest interval of i. | |
#define | SL_FLOOR(n, i) ((n / i) * i) |
Round n down to closest interval of i. | |
#define | STRINGIZE(X) #X |
Stringify X. | |
#define | SL_MIN(a, b) __extension__({ __typeof__(a)_a = (a); __typeof__(b)_b = (b); _a < _b ? _a : _b; }) |
A macro for getting the minimum value. | |
#define | SL_MAX(a, b) __extension__({ __typeof__(a)_a = (a); __typeof__(b)_b = (b); _a > _b ? _a : _b; }) |
A macro for getting the maximum value. | |
#define | SL_ATTRIBUTE_PACKED __attribute__ ((packed)) |
A GCC style macro for handling packed structures. | |
#define | SL_PACK_START(x) |
A macro for handling packed structures. | |
#define | SL_PACK_END() |
A macro for handling packed structures. | |
#define | SL_ATTRIBUTE_ALIGN(X) __attribute__ ((aligned(X))) |
GCC style macro for aligning a variable. | |
#define | SL_ALIGN(X) |
A macro for aligning a variable. | |
#define | SL_WEAK __attribute__ ((weak)) |
A macro for defining a weak symbol. | |
#define | SL_NORETURN __attribute__ ((noreturn)) |
A macro for handling non-returning functions. | |
#define | SL_ATTRIBUTE_SECTION(X) __attribute__ ((section(X))) |
A macro for placing a variable in a section. | |
#define | SL_FALLTHROUGH |
A macro for notifying the compiler of an intended switch case fallthrough. | |
#define | SL_DEPRECATED_API_SDK_3_0 __attribute__ ((deprecated)) |
Macro for marking deprecated functions. | |
Function Documentation
◆ SL_CTZ()
|
inline |
Count trailing number of zeros.
Use CLZ instruction if available.
- Parameters
-
[in] value
Data value to check for number of trailing zero bits.
- Returns
- A number of trailing zeros in value.
◆ SL_RBIT()
|
inline |
Reverse the bits.
Use the RBIT instruction if available, else process.
- Parameters
-
[in] value
Data value to reverse.
- Returns
- A reversed value.
◆ SL_RBIT16()
|
inline |
Reverse the bits.
Use the RBIT instruction if available, else process.
- Parameters
-
[in] value
16-bit data value to reverse.
- Returns
- A 16-bit reversed value.
◆ SL_Log2ToDiv()
|
inline |
Convert logarithm of 2 to division factor.
- Parameters
-
[in] log2
Logarithm of 2.
- Returns
- Dividend.
Macro Definition Documentation
◆ SL_CEILING
#define SL_CEILING | ( | n, |
|
i |
|||
) | ((((n) + (i) - 1U) / (i)) * (i)) |
Round n up to closest interval of i.
◆ SL_FLOOR
#define SL_FLOOR | ( | n, |
|
i |
|||
) | ((n / i) * i) |
Round n down to closest interval of i.
◆ STRINGIZE
#define STRINGIZE | ( | X | ) | #X |
Stringify X.
◆ SL_MIN
#define SL_MIN | ( | a, |
|
b |
|||
) | __extension__({ __typeof__(a)_a = (a); __typeof__(b)_b = (b); _a < _b ? _a : _b; }) |
A macro for getting the minimum value.
No sideeffects, a and b are evaluated one time only.
◆ SL_MAX
#define SL_MAX | ( | a, |
|
b |
|||
) | __extension__({ __typeof__(a)_a = (a); __typeof__(b)_b = (b); _a > _b ? _a : _b; }) |
A macro for getting the maximum value.
No sideeffects, a and b are evaluated one time only.
◆ SL_ATTRIBUTE_PACKED
#define SL_ATTRIBUTE_PACKED __attribute__ ((packed)) |
A GCC style macro for handling packed structures.
◆ SL_PACK_START
#define SL_PACK_START | ( | x | ) |
A macro for handling packed structures.
Use this macro before the structure definition.
X denotes the maximum alignment of structure members. X is not supported with GCC. GCC always uses 1 byte maximum alignment.
◆ SL_PACK_END
#define SL_PACK_END | ( |
| ) |
A macro for handling packed structures.
Use this macro after the structure definition.
With GCC, add SL_ATTRIBUTE_PACKED after the closing curly braces of the structure definition.
◆ SL_ATTRIBUTE_ALIGN
#define SL_ATTRIBUTE_ALIGN | ( | X | ) | __attribute__ ((aligned(X))) |
GCC style macro for aligning a variable.
◆ SL_ALIGN
#define SL_ALIGN | ( | X | ) |
A macro for aligning a variable.
Use this macro before the variable definition.
X denotes the storage alignment value in bytes.
To be GCC-compatible, use SL_ATTRIBUTE_ALIGN(X) before the semicolon on normal variables. Use SL_ATTRIBUTE_ALIGN(X) before the opening curly brace on structure variables.
◆ SL_WEAK
#define SL_WEAK __attribute__ ((weak)) |
A macro for defining a weak symbol.
◆ SL_NORETURN
#define SL_NORETURN __attribute__ ((noreturn)) |
A macro for handling non-returning functions.
◆ SL_ATTRIBUTE_SECTION
#define SL_ATTRIBUTE_SECTION | ( | X | ) | __attribute__ ((section(X))) |
A macro for placing a variable in a section.
Use this macro after the variable definition, before the equal sign or a semicolon.
X denotes the section to place the variable in.
◆ SL_FALLTHROUGH
#define SL_FALLTHROUGH |
A macro for notifying the compiler of an intended switch case fallthrough.
◆ SL_DEPRECATED_API_SDK_3_0
#define SL_DEPRECATED_API_SDK_3_0 __attribute__ ((deprecated)) |
Macro for marking deprecated functions.
SL_DEPRECATED_API_SDK_<RELEASE> is used to mark functions that are deprecated and should not be used from a given version of the SDK. The accompanying SL_SUPPRESS_DEPRECATION_WARNINGS_SDK_<RELEASE> define can be set to suppress warnings generated when using deprecated APIs.