WDOG_Init_TypeDef Struct Reference
Watchdog initialization structure.
#include <em_wdog.h>
Data Fields | |
bool | enable |
Enable watchdog when initialization completed. | |
bool | debugRun |
Counter keeps running during debug halt. | |
bool | em2Run |
Counter keeps running when in EM2. | |
bool | em3Run |
Counter keeps running when in EM3. | |
bool | em4Block |
Block EMU from entering EM4. | |
bool | swoscBlock |
Block SW from disabling LFRCO/LFXO oscillators. | |
bool | lock |
Block SW from modifying the configuration (a reset is needed to reconfigure). | |
WDOG_ClkSel_TypeDef | clkSel |
Clock source to use for watchdog. | |
WDOG_PeriodSel_TypeDef | perSel |
Watchdog timeout period. | |
Watchdog initialization structure.
Field Documentation
◆ enable
bool WDOG_Init_TypeDef::enable |
Enable watchdog when initialization completed.
◆ debugRun
bool WDOG_Init_TypeDef::debugRun |
Counter keeps running during debug halt.
◆ em2Run
bool WDOG_Init_TypeDef::em2Run |
Counter keeps running when in EM2.
◆ em3Run
bool WDOG_Init_TypeDef::em3Run |
Counter keeps running when in EM3.
◆ em4Block
bool WDOG_Init_TypeDef::em4Block |
Block EMU from entering EM4.
◆ swoscBlock
bool WDOG_Init_TypeDef::swoscBlock |
Block SW from disabling LFRCO/LFXO oscillators.
◆ lock
bool WDOG_Init_TypeDef::lock |
Block SW from modifying the configuration (a reset is needed to reconfigure).
◆ clkSel
WDOG_ClkSel_TypeDef WDOG_Init_TypeDef::clkSel |
Clock source to use for watchdog.
◆ perSel
WDOG_PeriodSel_TypeDef WDOG_Init_TypeDef::perSel |
Watchdog timeout period.