Direct_Receive_PluginEMDRV > EZRADIODRV > Plugin_System
Detailed Description
Direct receive plugin, see Plugin System Layer for detailed documentation.
.
Data Structures |
|
| struct | EZRADIODRV_DirectRxHandle |
|
EzRadio direct rx plug-in instance initialization and handler structure.
|
|
Macros |
|
| #define | EZRADIODRV_DIRECT_RECEIVE_PLUGIN_INIT_DEFAULT |
|
Configuration data for EzRadio direct rx plug-in.
|
|
Typedefs |
|
| typedef struct EZRADIODRV_DirectRxHandle | EZRADIODRV_DirectRxHandle_t |
|
EzRadio direct rx plug-in instance initialization and handler structure.
|
|
Functions |
|
| Ecode_t | ezradioStartDirectReceive ( EZRADIODRV_Handle_t radioHandle) |
|
Starts direct reception with the radio configurations from the radioHandle parameter.
|
|
| Ecode_t | ezradioStopDirectReceive (void) |
|
Stops direct reception.
|
|
Macro Definition Documentation
| #define EZRADIODRV_DIRECT_RECEIVE_PLUGIN_INIT_DEFAULT |
Configuration data for EzRadio direct rx plug-in.
Definition at line
73
of file
ezradio_direct_receive_plugin.h
.
Function Documentation
| Ecode_t ezradioStartDirectReceive | ( | EZRADIODRV_Handle_t |
radioHandle
|
) |
Starts direct reception with the radio configurations from the radioHandle parameter.
- Parameters
-
radioHandleHandler of the EzRadio driver instance where channel configuration is set.
- Returns
- ECODE_EMDRV_EZRADIODRV_OK on success. On failure an appropriate EZRADIODRV Ecode_t is returned.
Definition at line
56
of file
ezradio_direct_receive_plugin.c
.
References EZRADIODRV_DirectRxHandle::channel , EZRADIODRV_HandleData::directRx , ECODE_EMDRV_EZRADIODRV_ILLEGAL_HANDLE , ECODE_EMDRV_EZRADIODRV_OK , ezradio_get_int_status() , and ezradio_start_rx() .
| Ecode_t ezradioStopDirectReceive | ( | void |
|
) |
Stops direct reception.
- Returns
- ECODE_EMDRV_EZRADIODRV_OK on success. On failure an appropriate EZRADIODRV Ecode_t is returned.
Definition at line
81
of file
ezradio_direct_receive_plugin.c
.
References ECODE_EMDRV_EZRADIODRV_OK , and ezradio_change_state() .