EMU_TypeDef Struct ReferenceDevices > EFM32ZG_EMU
Definition at line 48
of file efm32zg_emu.h
.
Data Fields | |
__IOM uint32_t | AUXCTRL |
__IOM uint32_t | CTRL |
__IOM uint32_t | LOCK |
uint32_t | RESERVED0 [1] |
uint32_t | RESERVED1 [6] |
Field Documentation
__IOM uint32_t EMU_TypeDef::AUXCTRL |
Auxiliary Control Register
Definition at line 55
of file efm32zg_emu.h
.
__IOM uint32_t EMU_TypeDef::CTRL |
Control Register
Definition at line 49
of file efm32zg_emu.h
.
__IOM uint32_t EMU_TypeDef::LOCK |
Configuration Lock Register
Definition at line 52
of file efm32zg_emu.h
.
uint32_t EMU_TypeDef::RESERVED0[1] |
Reserved for future use
Definition at line 51
of file efm32zg_emu.h
.
uint32_t EMU_TypeDef::RESERVED1[6] |
Reserved for future use
Definition at line 54
of file efm32zg_emu.h
.
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32ZG/Include/
efm32zg_emu.h