PRS_TypeDef Struct ReferenceDevices > EFM32ZG_PRS
Definition at line 48
of file efm32zg_prs.h
.
Data Fields | |
PRS_CH_TypeDef | CH [4] |
uint32_t | RESERVED0 [1] |
__IOM uint32_t | ROUTE |
__IOM uint32_t | SWLEVEL |
__IOM uint32_t | SWPULSE |
Field Documentation
PRS_CH_TypeDef PRS_TypeDef::CH[4] |
Channel registers
Definition at line 54
of file efm32zg_prs.h
.
uint32_t PRS_TypeDef::RESERVED0[1] |
Reserved registers
Definition at line 53
of file efm32zg_prs.h
.
__IOM uint32_t PRS_TypeDef::ROUTE |
I/O Routing Register
Definition at line 51
of file efm32zg_prs.h
.
__IOM uint32_t PRS_TypeDef::SWLEVEL |
Software Level Register
Definition at line 50
of file efm32zg_prs.h
.
__IOM uint32_t PRS_TypeDef::SWPULSE |
Software Pulse Register
Definition at line 49
of file efm32zg_prs.h
.
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32ZG/Include/
efm32zg_prs.h