DMA_TypeDef Struct ReferenceDevices > EFM32ZG_DMA

Definition at line 48 of file efm32zg_dma.h .

Data Fields

__IM uint32_t ALTCTRLBASE
DMA_CH_TypeDef CH [4]
__OM uint32_t CHALTC
__IOM uint32_t CHALTS
__OM uint32_t CHENC
__IOM uint32_t CHENS
__OM uint32_t CHPRIC
__IOM uint32_t CHPRIS
__OM uint32_t CHREQMASKC
__IOM uint32_t CHREQMASKS
__IM uint32_t CHREQSTATUS
__IM uint32_t CHSREQSTATUS
__OM uint32_t CHSWREQ
__OM uint32_t CHUSEBURSTC
__IOM uint32_t CHUSEBURSTS
__IM uint32_t CHWAITSTATUS
__OM uint32_t CONFIG
__IOM uint32_t CTRLBASE
__IOM uint32_t ERRORC
__IOM uint32_t IEN
__IM uint32_t IF
__IOM uint32_t IFC
__IOM uint32_t IFS
uint32_t RESERVED0 [3]
uint32_t RESERVED1 [880]
uint32_t RESERVED2 [1]
uint32_t RESERVED3 [121]
uint32_t RESERVED4 [60]
__IM uint32_t STATUS

Field Documentation

__IM uint32_t DMA_TypeDef::ALTCTRLBASE

Channel Alternate Control Data Base Pointer Register

Definition at line 52 of file efm32zg_dma.h .

DMA_CH_TypeDef DMA_TypeDef::CH[4]

Channel registers

Definition at line 80 of file efm32zg_dma.h .

__OM uint32_t DMA_TypeDef::CHALTC

Channel Alternate Clear Register

Definition at line 62 of file efm32zg_dma.h .

__IOM uint32_t DMA_TypeDef::CHALTS

Channel Alternate Set Register

Definition at line 61 of file efm32zg_dma.h .

__OM uint32_t DMA_TypeDef::CHENC

Channel Enable Clear Register

Definition at line 60 of file efm32zg_dma.h .

__IOM uint32_t DMA_TypeDef::CHENS

Channel Enable Set Register

Definition at line 59 of file efm32zg_dma.h .

__OM uint32_t DMA_TypeDef::CHPRIC

Channel Priority Clear Register

Definition at line 64 of file efm32zg_dma.h .

__IOM uint32_t DMA_TypeDef::CHPRIS

Channel Priority Set Register

Definition at line 63 of file efm32zg_dma.h .

__OM uint32_t DMA_TypeDef::CHREQMASKC

Channel Request Mask Clear Register

Definition at line 58 of file efm32zg_dma.h .

__IOM uint32_t DMA_TypeDef::CHREQMASKS

Channel Request Mask Set Register

Definition at line 57 of file efm32zg_dma.h .

__IM uint32_t DMA_TypeDef::CHREQSTATUS

Channel Request Status

Definition at line 69 of file efm32zg_dma.h .

__IM uint32_t DMA_TypeDef::CHSREQSTATUS

Channel Single Request Status

Definition at line 71 of file efm32zg_dma.h .

__OM uint32_t DMA_TypeDef::CHSWREQ

Channel Software Request Register

Definition at line 54 of file efm32zg_dma.h .

__OM uint32_t DMA_TypeDef::CHUSEBURSTC

Channel Useburst Clear Register

Definition at line 56 of file efm32zg_dma.h .

__IOM uint32_t DMA_TypeDef::CHUSEBURSTS

Channel Useburst Set Register

Definition at line 55 of file efm32zg_dma.h .

__IM uint32_t DMA_TypeDef::CHWAITSTATUS

Channel Wait on Request Status Register

Definition at line 53 of file efm32zg_dma.h .

__OM uint32_t DMA_TypeDef::CONFIG

DMA Configuration Register

Definition at line 50 of file efm32zg_dma.h .

__IOM uint32_t DMA_TypeDef::CTRLBASE

Channel Control Data Base Pointer Register

Definition at line 51 of file efm32zg_dma.h .

__IOM uint32_t DMA_TypeDef::ERRORC

Bus Error Clear Register

Definition at line 66 of file efm32zg_dma.h .

__IOM uint32_t DMA_TypeDef::IEN

Interrupt Enable register

Definition at line 77 of file efm32zg_dma.h .

__IM uint32_t DMA_TypeDef::IF

Interrupt Flag Register

Definition at line 74 of file efm32zg_dma.h .

__IOM uint32_t DMA_TypeDef::IFC

Interrupt Flag Clear Register

Definition at line 76 of file efm32zg_dma.h .

__IOM uint32_t DMA_TypeDef::IFS

Interrupt Flag Set Register

Definition at line 75 of file efm32zg_dma.h .

uint32_t DMA_TypeDef::RESERVED0[3]

Reserved for future use

Definition at line 65 of file efm32zg_dma.h .

uint32_t DMA_TypeDef::RESERVED1[880]

Reserved for future use

Definition at line 68 of file efm32zg_dma.h .

uint32_t DMA_TypeDef::RESERVED2[1]

Reserved for future use

Definition at line 70 of file efm32zg_dma.h .

uint32_t DMA_TypeDef::RESERVED3[121]

Reserved for future use

Definition at line 73 of file efm32zg_dma.h .

uint32_t DMA_TypeDef::RESERVED4[60]

Reserved registers

Definition at line 79 of file efm32zg_dma.h .

__IM uint32_t DMA_TypeDef::STATUS

DMA Status Registers

Definition at line 49 of file efm32zg_dma.h .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32ZG/Include/ efm32zg_dma.h