RMU_TypeDef Struct ReferenceDevices > EFM32ZG_RMU
Definition at line 48
of file efm32zg_rmu.h
.
Data Fields | |
__OM uint32_t | CMD |
__IOM uint32_t | CTRL |
__IM uint32_t | RSTCAUSE |
Field Documentation
__OM uint32_t RMU_TypeDef::CMD |
Command Register
Definition at line 51
of file efm32zg_rmu.h
.
__IOM uint32_t RMU_TypeDef::CTRL |
Control Register
Definition at line 49
of file efm32zg_rmu.h
.
__IM uint32_t RMU_TypeDef::RSTCAUSE |
Reset Cause Register
Definition at line 50
of file efm32zg_rmu.h
.
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32ZG/Include/
efm32zg_rmu.h