IDAC_TypeDef Struct ReferenceDevices > EFM32ZG_IDAC
Definition at line 48
of file efm32zg_idac.h
.
Data Fields | |
__IOM uint32_t | CAL |
__IOM uint32_t | CTRL |
__IOM uint32_t | CURPROG |
__IOM uint32_t | DUTYCONFIG |
Field Documentation
__IOM uint32_t IDAC_TypeDef::CAL |
Calibration Register
Definition at line 51
of file efm32zg_idac.h
.
Referenced by IDAC_RangeSet(), and IDAC_Reset().
__IOM uint32_t IDAC_TypeDef::CTRL |
Control Register
Definition at line 49
of file efm32zg_idac.h
.
Referenced by IDAC_Enable(), IDAC_Init(), IDAC_MinimalOutputTransitionMode(), IDAC_OutEnable(), IDAC_RangeSet(), and IDAC_Reset().
__IOM uint32_t IDAC_TypeDef::CURPROG |
Current Programming Register
Definition at line 50
of file efm32zg_idac.h
.
Referenced by IDAC_RangeSet(), IDAC_Reset(), and IDAC_StepSet().
__IOM uint32_t IDAC_TypeDef::DUTYCONFIG |
Duty Cycle Configauration Register
Definition at line 52
of file efm32zg_idac.h
.
Referenced by IDAC_Reset().
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32ZG/Include/
efm32zg_idac.h