ADC_TypeDef Struct ReferenceDevices > EFM32ZG_ADC
Definition at line 48
of file efm32zg_adc.h
.
Data Fields | |
__IOM uint32_t | BIASPROG |
__IOM uint32_t | CAL |
__IOM uint32_t | CMD |
__IOM uint32_t | CTRL |
__IOM uint32_t | IEN |
__IM uint32_t | IF |
__IOM uint32_t | IFC |
__IOM uint32_t | IFS |
uint32_t | RESERVED0 [1] |
__IOM uint32_t | SCANCTRL |
__IM uint32_t | SCANDATA |
__IM uint32_t | SCANDATAP |
__IOM uint32_t | SINGLECTRL |
__IM uint32_t | SINGLEDATA |
__IM uint32_t | SINGLEDATAP |
__IM uint32_t | STATUS |
Field Documentation
__IOM uint32_t ADC_TypeDef::BIASPROG |
Bias Programming Register
Definition at line 65
of file efm32zg_adc.h
.
Referenced by ADC_InitSingle(), and ADC_Reset().
__IOM uint32_t ADC_TypeDef::CAL |
Calibration Register
Definition at line 62
of file efm32zg_adc.h
.
__IOM uint32_t ADC_TypeDef::CMD |
Command Register
Definition at line 50
of file efm32zg_adc.h
.
Referenced by ADC_Init(), ADC_InitScan(), ADC_InitSingle(), ADC_Reset(), and ADC_Start().
__IOM uint32_t ADC_TypeDef::CTRL |
Control Register
Definition at line 49
of file efm32zg_adc.h
.
Referenced by ADC_Init(), ADC_InitScan(), ADC_InitSingle(), and ADC_Reset().
__IOM uint32_t ADC_TypeDef::IEN |
Interrupt Enable Register
Definition at line 54
of file efm32zg_adc.h
.
Referenced by ADC_IntDisable(), ADC_IntEnable(), ADC_IntGetEnabled(), and ADC_Reset().
__IM uint32_t ADC_TypeDef::IF |
Interrupt Flag Register
Definition at line 55
of file efm32zg_adc.h
.
Referenced by ADC_IntGet(), and ADC_IntGetEnabled().
__IOM uint32_t ADC_TypeDef::IFC |
Interrupt Flag Clear Register
Definition at line 57
of file efm32zg_adc.h
.
Referenced by ADC_IntClear(), and ADC_Reset().
__IOM uint32_t ADC_TypeDef::IFS |
Interrupt Flag Set Register
Definition at line 56
of file efm32zg_adc.h
.
Referenced by ADC_IntSet().
uint32_t ADC_TypeDef::RESERVED0[1] |
Reserved for future use
Definition at line 64
of file efm32zg_adc.h
.
__IOM uint32_t ADC_TypeDef::SCANCTRL |
Scan Control Register
Definition at line 53
of file efm32zg_adc.h
.
Referenced by ADC_InitScan(), and ADC_Reset().
__IM uint32_t ADC_TypeDef::SCANDATA |
Scan Conversion Result Data
Definition at line 59
of file efm32zg_adc.h
.
Referenced by ADC_DataScanGet().
__IM uint32_t ADC_TypeDef::SCANDATAP |
Scan Sequence Result Data Peek Register
Definition at line 61
of file efm32zg_adc.h
.
Referenced by ADC_DataScanPeek().
__IOM uint32_t ADC_TypeDef::SINGLECTRL |
Single Sample Control Register
Definition at line 52
of file efm32zg_adc.h
.
Referenced by ADC_InitSingle(), and ADC_Reset().
__IM uint32_t ADC_TypeDef::SINGLEDATA |
Single Conversion Result Data
Definition at line 58
of file efm32zg_adc.h
.
Referenced by ADC_DataSingleGet().
__IM uint32_t ADC_TypeDef::SINGLEDATAP |
Single Conversion Result Data Peek Register
Definition at line 60
of file efm32zg_adc.h
.
Referenced by ADC_DataSinglePeek().
__IM uint32_t ADC_TypeDef::STATUS |
Status Register
Definition at line 51
of file efm32zg_adc.h
.
Referenced by ADC_InitScan(), and ADC_InitSingle().
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32ZG/Include/
efm32zg_adc.h