NandFlashKit Drivers
Detailed Description
Implements a NAND flash device driver. The driver has basic functions to read and write data to a nand flash device.
When writing to the nand flash, an ECC is generated and written in the page spare area. This ECC is checked when the page is read and the data read is corrected when possible. Read and write operations can be done using DMA (configurable) at initialization.
The module is easily adapted to other NAND flash devices.
Data Structures |
|
| struct | NANDFLASH_Info_TypeDef |
|
NANDFLASH device information structure.
|
|
Macros |
|
| #define | NAND256W3A_SPARESIZE 16 |
| #define | NAND_SPARE_BADBLOCK_POS 5 |
| #define | NAND_SPARE_ECC0_POS 6 |
| #define | NAND_SPARE_ECC1_POS 7 |
| #define | NAND_SPARE_ECC2_POS 8 |
Enumerations |
|
| enum |
NANDFLASH_Status_TypeDef
{
NANDFLASH_STATUS_OK = 0, NANDFLASH_INVALID_DEVICE = -1, NANDFLASH_INVALID_ADDRESS = -2, NANDFLASH_WRITE_ERROR = -3, NANDFLASH_ECC_ERROR = -4, NANDFLASH_ECC_UNCORRECTABLE = -5, NANDFLASH_INVALID_SETUP = -6, NANDFLASH_NOT_INITIALIZED = -7 } |
|
NANDFLASH status enumerator.
|
|
Functions |
|
| bool | NANDFLASH_AddressValid (uint32_t addr) |
|
Check if an address is valid for the nand flash device.
|
|
| int | NANDFLASH_CopyPage (uint32_t dstAddr, uint32_t srcAddr) |
|
Copy a page within the device to a new location.
|
|
| NANDFLASH_Info_TypeDef * | NANDFLASH_DeviceInfo (void) |
|
Return a pointer to a
NANDFLASH_Info_TypeDef
structure, which contain vital nand flash device information.
|
|
| int | NANDFLASH_EccCorrect (uint32_t generatedEcc, uint32_t readEcc, uint8_t *data) |
|
Check generated ECC against ECC read from device and correct data if possible.
|
|
| int | NANDFLASH_EraseBlock (uint32_t address) |
|
Erase a block in the nand flash.
|
|
| int | NANDFLASH_Init (int dmaCh) |
|
Initialize the NANDFLASH module.
|
|
| int | NANDFLASH_MarkBadBlock (uint32_t address) |
|
Mark a block as bad.
|
|
| int | NANDFLASH_ReadPage (uint32_t address, uint8_t *buffer) |
|
Read a page from nand device. Ecc errors will be detected and corrected if possible.
NANDFLASH_Info_TypeDef::ecc
will be set to the ecc generated while reading the page data.
NANDFLASH_Info_TypeDef::spare
will be set to the content of the page spare area.
|
|
| int | NANDFLASH_ReadSpare (uint32_t address, uint8_t *buffer) |
|
Read the spare area content of a page.
|
|
| int | NANDFLASH_WritePage (uint32_t address, uint8_t *buffer) |
|
Write a page in nand device. The ECC generated while writing the page data is written in the spare area at byte positions 7, 8 and 9.
|
|
Macro Definition Documentation
| #define NAND256W3A_SPARESIZE 16 |
Spare area size of Numonyx NAND256W3A.
Definition at line
33
of file
nandflash.h
.
| #define NAND_SPARE_BADBLOCK_POS 5 |
Spare area position of bad-block marker.
Definition at line
36
of file
nandflash.h
.
| #define NAND_SPARE_ECC0_POS 6 |
Spare area position of ECC byte 0 (LSB).
Definition at line
37
of file
nandflash.h
.
Referenced by NANDFLASH_ReadPage() .
| #define NAND_SPARE_ECC1_POS 7 |
Spare area position of ECC byte 1.
Definition at line
38
of file
nandflash.h
.
Referenced by NANDFLASH_ReadPage() .
| #define NAND_SPARE_ECC2_POS 8 |
Spare area position of ECC byte 2 (MSB).
Definition at line
39
of file
nandflash.h
.
Referenced by NANDFLASH_ReadPage() .
Enumeration Type Documentation
NANDFLASH status enumerator.
| Enumerator | |
|---|---|
| NANDFLASH_STATUS_OK |
No errors detected. |
| NANDFLASH_INVALID_DEVICE |
Invalid (unsupported) flash device. |
| NANDFLASH_INVALID_ADDRESS |
Invalid nand flash address. |
| NANDFLASH_WRITE_ERROR |
Nand flash write error, block is "bad". |
| NANDFLASH_ECC_ERROR |
Illegal ECC value read from spare area. |
| NANDFLASH_ECC_UNCORRECTABLE |
Uncorrectable data error in page. |
| NANDFLASH_INVALID_SETUP |
Invalid parameter to NANDFLASH_Init() . |
| NANDFLASH_NOT_INITIALIZED |
Nand module has not been initialized. |
Definition at line
42
of file
nandflash.h
.
Function Documentation
| bool NANDFLASH_AddressValid | ( | uint32_t |
address
|
) |
Check if an address is valid for the nand flash device.
- Parameters
-
[in] addressThe address value to check.
- Returns
- True if address value is valid, false otherwise.
Definition at line
154
of file
nandflash.c
.
References NANDFLASH_Info_TypeDef::baseAddress , and NANDFLASH_Info_TypeDef::deviceSize .
Referenced by NANDFLASH_CopyPage() , NANDFLASH_EraseBlock() , NANDFLASH_MarkBadBlock() , NANDFLASH_ReadPage() , NANDFLASH_ReadSpare() , and NANDFLASH_WritePage() .
| int NANDFLASH_CopyPage | ( | uint32_t |
dstAddr,
|
| uint32_t |
srcAddr
|
||
| ) |
Copy a page within the device to a new location.
- Parameters
-
[in] dstAddrThe address of the destination page.
- Note
- The copy operation is performed inside the nand flash. No data is read from or written to the device.
- Parameters
-
[in] srcAddrThe address of the source page.
- Returns
- NANDFLASH_STATUS_OK on success, an error code enumerated in NANDFLASH_Status_TypeDef on failure.
Definition at line
184
of file
nandflash.c
.
References NANDFLASH_AddressValid() , NANDFLASH_INVALID_ADDRESS , NANDFLASH_NOT_INITIALIZED , NANDFLASH_STATUS_OK , and NANDFLASH_WRITE_ERROR .
| NANDFLASH_Info_TypeDef * NANDFLASH_DeviceInfo | ( | void |
|
) |
Return a pointer to a NANDFLASH_Info_TypeDef structure, which contain vital nand flash device information.
- Returns
- NULL if no prior call to NANDFLASH_Init() has been made. Pointer to a NANDFLASH_Info_TypeDef on success.
Definition at line
242
of file
nandflash.c
.
| int NANDFLASH_EccCorrect | ( | uint32_t |
generatedEcc,
|
| uint32_t |
readEcc,
|
||
| uint8_t * |
data
|
||
| ) |
Check generated ECC against ECC read from device and correct data if possible.
- Parameters
-
[in] generatedEccAn ECC value originating from the hardware ECC generator. [in] readEccAn ECC value read from a page spare area. [in] dataPointer to a page of data read from device.
- Returns
- NANDFLASH_STATUS_OK on success, an error code enumerated in NANDFLASH_Status_TypeDef on failure.
Definition at line
268
of file
nandflash.c
.
References NANDFLASH_ECC_ERROR , NANDFLASH_ECC_UNCORRECTABLE , and NANDFLASH_STATUS_OK .
Referenced by NANDFLASH_ReadPage() .
| int NANDFLASH_EraseBlock | ( | uint32_t |
address
|
) |
Erase a block in the nand flash.
- Note
- If this function returns NANDFLASH_WRITE_ERROR , the block should be considered as "bad" and never used again.
- Parameters
-
[in] addressBlock address.
- Returns
- NANDFLASH_STATUS_OK on success, an error code enumerated in NANDFLASH_Status_TypeDef on failure.
Definition at line
346
of file
nandflash.c
.
References NANDFLASH_AddressValid() , NANDFLASH_INVALID_ADDRESS , NANDFLASH_NOT_INITIALIZED , NANDFLASH_STATUS_OK , and NANDFLASH_WRITE_ERROR .
| int NANDFLASH_Init | ( | int |
dmaCh
|
) |
Initialize the NANDFLASH module.
- Note
- This function should be called before any other NANDFLASH_xxx() functions are used.
- Parameters
-
[in] dmaChThe DMA channel to use when transfering data to/from the device. DMA will not be used for data transfers if dmaCh is set to -1.
- Returns
- NANDFLASH_STATUS_OK on success, an error code enumerated in NANDFLASH_Status_TypeDef on failure.
Definition at line
398
of file
nandflash.c
.
References DMA_CfgChannel() , DMA_CHAN_COUNT , DMA_Init() , NANDFLASH_Info_TypeDef::dmaCh , and NANDFLASH_INVALID_SETUP .
| int NANDFLASH_MarkBadBlock | ( | uint32_t |
address
|
) |
Mark a block as bad.
- Note
- This function writes a bad-block marker in the spare area of the first page in the block. The marker is written in the 6th byte of the spare area. A bad-block marker is any value different from 0xFF.
- Parameters
-
[in] addressBlock address.
- Returns
- NANDFLASH_STATUS_OK on success, an error code enumerated in NANDFLASH_Status_TypeDef on failure.
Definition at line
431
of file
nandflash.c
.
References NANDFLASH_AddressValid() , NANDFLASH_INVALID_ADDRESS , NANDFLASH_NOT_INITIALIZED , and NANDFLASH_STATUS_OK .
| int NANDFLASH_ReadPage | ( | uint32_t |
address,
|
| uint8_t * |
buffer
|
||
| ) |
Read a page from nand device. Ecc errors will be detected and corrected if possible. NANDFLASH_Info_TypeDef::ecc will be set to the ecc generated while reading the page data. NANDFLASH_Info_TypeDef::spare will be set to the content of the page spare area.
- Parameters
-
[in] addressPage address. [in] bufferPointer to page data buffer.
- Returns
- NANDFLASH_STATUS_OK on success, an error code enumerated in NANDFLASH_Status_TypeDef on failure.
Definition at line
487
of file
nandflash.c
.
References NANDFLASH_Info_TypeDef::dmaCh , NANDFLASH_Info_TypeDef::ecc , NAND_SPARE_ECC0_POS , NAND_SPARE_ECC1_POS , NAND_SPARE_ECC2_POS , NANDFLASH_AddressValid() , NANDFLASH_EccCorrect() , NANDFLASH_INVALID_ADDRESS , NANDFLASH_NOT_INITIALIZED , NANDFLASH_Info_TypeDef::pageSize , NANDFLASH_Info_TypeDef::spare , and NANDFLASH_Info_TypeDef::spareSize .
| int NANDFLASH_ReadSpare | ( | uint32_t |
address,
|
| uint8_t * |
buffer
|
||
| ) |
Read the spare area content of a page.
- Parameters
-
[in] addressPage address. [in] bufferPointer to page spare area data buffer.
- Returns
- NANDFLASH_STATUS_OK on success, an error code enumerated in NANDFLASH_Status_TypeDef on failure.
Definition at line
558
of file
nandflash.c
.
References NANDFLASH_Info_TypeDef::dmaCh , NANDFLASH_AddressValid() , NANDFLASH_INVALID_ADDRESS , NANDFLASH_NOT_INITIALIZED , NANDFLASH_STATUS_OK , and NANDFLASH_Info_TypeDef::spareSize .
| int NANDFLASH_WritePage | ( | uint32_t |
address,
|
| uint8_t * |
buffer
|
||
| ) |
Write a page in nand device. The ECC generated while writing the page data is written in the spare area at byte positions 7, 8 and 9.
- Note
- If this function returns NANDFLASH_WRITE_ERROR , the block should be considered as "bad" and never used again.
- Parameters
-
[in] addressPage address. [in] bufferPointer to page data buffer.
- Returns
- NANDFLASH_STATUS_OK on success, an error code enumerated in NANDFLASH_Status_TypeDef on failure.
Definition at line
617
of file
nandflash.c
.
References NANDFLASH_Info_TypeDef::dmaCh , NANDFLASH_Info_TypeDef::ecc , NANDFLASH_AddressValid() , NANDFLASH_INVALID_ADDRESS , NANDFLASH_NOT_INITIALIZED , NANDFLASH_STATUS_OK , NANDFLASH_WRITE_ERROR , and NANDFLASH_Info_TypeDef::pageSize .