CMU_HFXOInit_TypeDef Struct ReferenceEMLIB > CMU
HFXO initialization structure. Init values should be obtained from a configuration tool, app note or xtal datasheet
Definition at line
1395
of file
em_cmu.h
.
#include <
em_cmu.h
>
Data Fields |
|
| uint8_t | boost |
| bool | glitchDetector |
| CMU_OscMode_TypeDef | mode |
| uint8_t | timeout |
Field Documentation
| uint8_t CMU_HFXOInit_TypeDef::boost |
HFXO Boost, 0=50% 1=70%, 2=80%, 3=100%
Definition at line
1420
of file
em_cmu.h
.
Referenced by CMU_HFXOInit() .
| bool CMU_HFXOInit_TypeDef::glitchDetector |
Enable/disable glitch detector
Definition at line
1422
of file
em_cmu.h
.
Referenced by CMU_HFXOInit() .
| CMU_OscMode_TypeDef CMU_HFXOInit_TypeDef::mode |
| uint8_t CMU_HFXOInit_TypeDef::timeout |
The documentation for this struct was generated from the following file:
-
C:/repos/embsw_super_h1/platform/emlib/inc/
em_cmu.h