SYSTEM_CalAddrVal_TypeDef Struct ReferenceEMLIB > SYSTEM
DEVINFO calibration address/value pair
Definition at line 275
of file em_system.h
.
#include <
em_system.h
>
Data Fields | |
uint32_t | address |
uint32_t | calValue |
Field Documentation
uint32_t SYSTEM_CalAddrVal_TypeDef::address |
Peripheral calibration register address
Definition at line 276
of file em_system.h
.
Referenced by SYSTEM_GetCalibrationValue().
uint32_t SYSTEM_CalAddrVal_TypeDef::calValue |
Calibration value for register at address
Definition at line 277
of file em_system.h
.
Referenced by SYSTEM_GetCalibrationValue().
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/emlib/inc/
em_system.h