SMUEMLIB
Detailed Description
Security Management Unit (SMU) Peripheral API.
The Security Management Unit (SMU) forms the control and status/reporting component of bus-level security in EFM32/EFR32 devices.
Peripheral-level protection is provided via the peripheral protection unit (PPU). The PPU provides a hardware access barrier to any peripheral that is configured to be protected. When an attempt is made to access a peripheral without the required privilege/security level, the PPU detects the fault and intercepts the access. No write or read of the peripheral register space occurs, and an all-zero value is returned if the access is a read.
         Data Structures | 
       |
| struct | SMU_Init_TypeDef | 
| struct | SMU_PrivilegedAccess_TypeDef | 
         Macros | 
       |
| #define | SMU_INIT_DEFAULT | 
         Enumerations | 
       |
| enum | 
         
          SMU_Peripheral_TypeDef
         
         {
          smuPeripheralACMP0 = _SMU_PPUPATD0_ACMP0_SHIFT, smuPeripheralACMP1 = _SMU_PPUPATD0_ACMP1_SHIFT, smuPeripheralADC0 = _SMU_PPUPATD0_ADC0_SHIFT, smuPeripheralCMU = _SMU_PPUPATD0_CMU_SHIFT, smuPeripheralCRYOTIMER = _SMU_PPUPATD0_CRYOTIMER_SHIFT, smuPeripheralCRYPTO = _SMU_PPUPATD0_CRYPTO0_SHIFT, smuPeripheralVDAC0 = _SMU_PPUPATD0_VDAC0_SHIFT, smuPeripheralPRS = _SMU_PPUPATD0_PRS_SHIFT, smuPeripheralEMU = _SMU_PPUPATD0_EMU_SHIFT, smuPeripheralFPUEH = _SMU_PPUPATD0_FPUEH_SHIFT, smuPeripheralGPCRC = _SMU_PPUPATD0_GPCRC_SHIFT, smuPeripheralGPIO = _SMU_PPUPATD0_GPIO_SHIFT, smuPeripheralI2C0 = _SMU_PPUPATD0_I2C0_SHIFT, smuPeripheralIDAC0 = _SMU_PPUPATD0_IDAC0_SHIFT, smuPeripheralMSC = _SMU_PPUPATD0_MSC_SHIFT, smuPeripheralLDMA = _SMU_PPUPATD0_LDMA_SHIFT, smuPeripheralLESENSE = _SMU_PPUPATD0_LESENSE_SHIFT, smuPeripheralLETIMER0 = _SMU_PPUPATD0_LETIMER0_SHIFT, smuPeripheralLEUART = _SMU_PPUPATD0_LEUART0_SHIFT, smuPeripheralPCNT0 = _SMU_PPUPATD0_PCNT0_SHIFT, smuPeripheralRMU = _SMU_PPUPATD0_RMU_SHIFT, smuPeripheralRTCC = _SMU_PPUPATD0_RTCC_SHIFT, smuPeripheralSMU = _SMU_PPUPATD0_SMU_SHIFT, smuPeripheralTIMER0 = 32 + _SMU_PPUPATD1_TIMER0_SHIFT, smuPeripheralTIMER1 = 32 + _SMU_PPUPATD1_TIMER1_SHIFT, smuPeripheralTRNG0 = 32 + _SMU_PPUPATD1_TRNG0_SHIFT, smuPeripheralUSART0 = 32 + _SMU_PPUPATD1_USART0_SHIFT, smuPeripheralUSART1 = 32 + _SMU_PPUPATD1_USART1_SHIFT, smuPeripheralWDOG0 = 32 + _SMU_PPUPATD1_WDOG0_SHIFT, smuPeripheralWDOG1 = 32 + _SMU_PPUPATD1_WDOG1_SHIFT, smuPeripheralWTIMER0 = 32 + _SMU_PPUPATD1_WTIMER0_SHIFT, smuPeripheralEnd }  | 
       
         Functions | 
       |
| __STATIC_INLINE void | SMU_EnablePPU (bool enable) | 
| 
         Enable or disable the Peripheral Protection Unit of the SMU.
          | 
       |
| __STATIC_INLINE SMU_Peripheral_TypeDef | SMU_GetFaultingPeripheral (void) | 
| 
         Get the ID of the peripheral that caused an access fault.
          | 
       |
| __STATIC_INLINE void | SMU_Init (const SMU_Init_TypeDef *init) | 
| 
         Initialize the Peripheral Protection Unit of the SMU.
          | 
       |
| __STATIC_INLINE void | SMU_IntClear (uint32_t flags) | 
| 
         Clear one or more pending SMU interrupts.
          | 
       |
| __STATIC_INLINE void | SMU_IntDisable (uint32_t flags) | 
| 
         Disable one or more SMU interrupts.
          | 
       |
| __STATIC_INLINE void | SMU_IntEnable (uint32_t flags) | 
| 
         Enable one or more SMU interrupts.
          | 
       |
| __STATIC_INLINE uint32_t | SMU_IntGet (void) | 
| 
         Get pending SMU interrupts.
          | 
       |
| __STATIC_INLINE uint32_t | SMU_IntGetEnabled (void) | 
| 
         Get enabled and pending SMU interrupt flags. Useful for handling more interrupt sources in the same interrupt handler.
          | 
       |
| __STATIC_INLINE void | SMU_IntSet (uint32_t flags) | 
| 
         Set one or more pending SMU interrupts from SW.
          | 
       |
| __STATIC_INLINE void | SMU_SetPrivilegedAccess ( SMU_Peripheral_TypeDef peripheral, bool privileged) | 
| 
         Change the access settings for a peripheral.
          | 
       |
Macro Definition Documentation
| #define SMU_INIT_DEFAULT | 
Default SMU initialization struct settings.
        Definition at line
        
         597
        
        of file
        
         em_smu.h
        
        .
       
Enumeration Type Documentation
SMU peripheral identifiers.
        Definition at line
        
         79
        
        of file
        
         em_smu.h
        
        .
       
Function Documentation
| __STATIC_INLINE void SMU_EnablePPU | ( | bool | 
           
            enable
           
           | 
          ) | 
Enable or disable the Peripheral Protection Unit of the SMU.
- Parameters
 - 
         
[in] enableTrue if the PPU should be enabled, false if it should be disabled.  
        Definition at line
        
         613
        
        of file
        
         em_smu.h
        
        .
       
References _SMU_PPUCTRL_ENABLE_SHIFT , BUS_RegBitWrite() , and SMU .
Referenced by SMU_Init() .
| __STATIC_INLINE SMU_Peripheral_TypeDef SMU_GetFaultingPeripheral | ( | void | 
           
           
           | 
          ) | 
Get the ID of the peripheral that caused an access fault.
- Note
 - The return value is only valid if the SMU_IF_PPUPRIV interrupt flag is set.
 
- Returns
 - ID of the faulting peripheral.
 
        Definition at line
        
         672
        
        of file
        
         em_smu.h
        
        .
       
References SMU .
| __STATIC_INLINE void SMU_Init | ( | const SMU_Init_TypeDef * | 
           
            init
           
           | 
          ) | 
Initialize the Peripheral Protection Unit of the SMU.
- Parameters
 - 
         
[in] initPointer to initialization struct defining which peripherals should only be accessed from privileged mode, and whether the PPU should be enabled.  
        Definition at line
        
         626
        
        of file
        
         em_smu.h
        
        .
       
References SMU_Init_TypeDef::enable , SMU_Init_TypeDef::reg , SMU , and SMU_EnablePPU() .
| __STATIC_INLINE void SMU_IntClear | ( | uint32_t | 
           
            flags
           
           | 
          ) | 
Clear one or more pending SMU interrupts.
- Parameters
 - 
         
[in] flagsBitwise logic OR of SMU interrupt sources to clear.  
        Definition at line
        
         684
        
        of file
        
         em_smu.h
        
        .
       
References SMU .
| __STATIC_INLINE void SMU_IntDisable | ( | uint32_t | 
           
            flags
           
           | 
          ) | 
Disable one or more SMU interrupts.
- Parameters
 - 
         
[in] flagsSMU interrupt sources to disable.  
        Definition at line
        
         696
        
        of file
        
         em_smu.h
        
        .
       
References SMU .
| __STATIC_INLINE void SMU_IntEnable | ( | uint32_t | 
           
            flags
           
           | 
          ) | 
Enable one or more SMU interrupts.
- Note
 - Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. Consider using SMU_IntClear() prior to enabling if such a pending interrupt should be ignored.
 
- Parameters
 - 
         
[in] flagsSMU interrupt sources to enable.  
        Definition at line
        
         713
        
        of file
        
         em_smu.h
        
        .
       
References SMU .
| __STATIC_INLINE uint32_t SMU_IntGet | ( | void | 
           
           
           | 
          ) | 
Get pending SMU interrupts.
- Returns
 - SMU interrupt sources pending.
 
        Definition at line
        
         725
        
        of file
        
         em_smu.h
        
        .
       
References SMU .
| __STATIC_INLINE uint32_t SMU_IntGetEnabled | ( | void | 
           
           
           | 
          ) | 
Get enabled and pending SMU interrupt flags. Useful for handling more interrupt sources in the same interrupt handler.
- Note
 - Interrupt flags are not cleared by the use of this function.
 
- Returns
 - 
         Pending and enabled SMU interrupt sources. The return value is the bitwise AND combination of
         
- the OR combination of enabled interrupt sources in SMU_IEN register and
 - the OR combination of valid interrupt flags in SMU_IF register.
 
 
        Definition at line
        
         745
        
        of file
        
         em_smu.h
        
        .
       
References SMU .
| __STATIC_INLINE void SMU_IntSet | ( | uint32_t | 
           
            flags
           
           | 
          ) | 
Set one or more pending SMU interrupts from SW.
- Parameters
 - 
         
[in] flagsSMU interrupt sources to set to pending. Æ  
        Definition at line
        
         764
        
        of file
        
         em_smu.h
        
        .
       
References SMU .
| __STATIC_INLINE void SMU_SetPrivilegedAccess | ( | SMU_Peripheral_TypeDef | 
           
            peripheral,
           
           | 
         
| bool | 
           
            privileged
           
           | 
         ||
| ) | 
Change the access settings for a peripheral.
Set whether the peripheral can only be accessed from privileged mode
- Parameters
 - 
         
[in] peripheralID of the peripheral to change access settings for [in] privilegedTrue if the peripheral should only be allowed to be accessed from privileged mode, false if the peripheral can be accessed from unprivileged mode.  
        Definition at line
        
         649
        
        of file
        
         em_smu.h
        
        .
       
References BUS_RegBitWrite() , and SMU .