LESENSE_ConfAltEx_TypeDef Struct ReferenceEMLIB > LESENSE
Configuration structure for alternate excitation.
       Definition at line
       
        945
       
       of file
       
        em_lesense.h
       
       .
      
      
       #include <
       
     
        em_lesense.h
       
       >
      
         Data Fields | 
       |
| LESENSE_AltExDesc_TypeDef | AltEx [16] | 
| LESENSE_AltExMap_TypeDef | altExMap | 
Field Documentation
| LESENSE_AltExDesc_TypeDef LESENSE_ConfAltEx_TypeDef::AltEx[16] | 
Alternate excitation channel descriptors. When altExMap==lesenseAltExMapALTEX only the 8 first descriptors are used. In this mode they describe the configuration of the LES_ALTEX0-7 pins. When altExMap==lesenseAltExMapACMP all 16 descriptors are used. In this mode they describe the configuration of the 16 possible ACMP0-1 excitation channels. Please refer to the user manual for a complete mapping of the routing. NOTE: Some parameters in the descriptors are not valid when altExMap==lesenseAltExMapACMP. Please refer to the definition of the LESENSE_AltExDesc_TypeDef structure for details regarding which parameters are valid.
        Definition at line
        
         961
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_AltExConfig() .
| LESENSE_AltExMap_TypeDef LESENSE_ConfAltEx_TypeDef::altExMap | 
Select alternate excitation mapping.
        Definition at line
        
         947
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_AltExConfig() .
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/emlib/inc/
       
em_lesense.h