NORFLASH_Info_TypeDef Struct ReferenceKit Drivers > NorFlash

NORFLASH device information struct.

Definition at line 49 of file norflash.h.

#include <norflash.h>

Data Fields

uint32_t baseAddress
 
uint32_t deviceId
 
uint32_t deviceSize
 
uint16_t manufacturerId
 
uint32_t sectorCount
 
uint32_t sectorSize
 

Field Documentation

uint32_t NORFLASH_Info_TypeDef::baseAddress

The device base address in cpu memory map.

Definition at line 50 of file norflash.h.

Referenced by NORFLASH_AddressValid(), and NORFLASH_EraseDevice().

uint32_t NORFLASH_Info_TypeDef::deviceId

The device ID.

Definition at line 51 of file norflash.h.

uint32_t NORFLASH_Info_TypeDef::deviceSize

Total device size in bytes.

Definition at line 52 of file norflash.h.

Referenced by NORFLASH_AddressValid().

uint16_t NORFLASH_Info_TypeDef::manufacturerId

The device manufacturer ID.

Definition at line 55 of file norflash.h.

uint32_t NORFLASH_Info_TypeDef::sectorCount

Number of sectors in the device.

Definition at line 53 of file norflash.h.

uint32_t NORFLASH_Info_TypeDef::sectorSize

Sector size in bytes.

Definition at line 54 of file norflash.h.

Referenced by NORFLASH_EraseSector(), and NORFLASH_Program().


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/hardware/kit/common/drivers/norflash.h