EMU_TypeDef Struct ReferenceDevices > EMU
EMU Register Declaration
       Definition at line
       
        49
       
       of file
       
        efr32bg14p_emu.h
       
       .
      
      
       #include <
       
     
        efr32bg14p_emu.h
       
       >
      
         Data Fields | 
       |
| __IOM uint32_t | CMD | 
| __IOM uint32_t | CTRL | 
| __IOM uint32_t | DCDCCLIMCTRL | 
| __IOM uint32_t | DCDCCTRL | 
| __IOM uint32_t | DCDCLNCOMPCTRL | 
| __IOM uint32_t | DCDCLNFREQCTRL | 
| __IOM uint32_t | DCDCLNVCTRL | 
| __IOM uint32_t | DCDCLPCTRL | 
| __IOM uint32_t | DCDCLPEM01CFG | 
| __IOM uint32_t | DCDCLPVCTRL | 
| __IOM uint32_t | DCDCMISCCTRL | 
| __IM uint32_t | DCDCSYNC | 
| __IOM uint32_t | DCDCZDETCTRL | 
| __IOM uint32_t | EM23PERNORETAINCMD | 
| __IOM uint32_t | EM23PERNORETAINCTRL | 
| __IM uint32_t | EM23PERNORETAINSTATUS | 
| __IOM uint32_t | EM4CTRL | 
| __IOM uint32_t | IEN | 
| __IM uint32_t | IF | 
| __IOM uint32_t | IFC | 
| __IOM uint32_t | IFS | 
| __IOM uint32_t | LOCK | 
| __IOM uint32_t | PWRCTRL | 
| __IOM uint32_t | PWRLOCK | 
| __IOM uint32_t | RAM0CTRL | 
| __IOM uint32_t | RAM1CTRL | 
| __IOM uint32_t | RAM2CTRL | 
| uint32_t | RESERVED0 [1] | 
| uint32_t | RESERVED1 [1] | 
| uint32_t | RESERVED2 [2] | 
| uint32_t | RESERVED3 [1] | 
| uint32_t | RESERVED4 [1] | 
| uint32_t | RESERVED5 [1] | 
| uint32_t | RESERVED6 [5] | 
| uint32_t | RESERVED7 [5] | 
| uint32_t | RESERVED8 [12] | 
| uint32_t | RESERVED9 [4] | 
| __IM uint32_t | STATUS | 
| __IM uint32_t | TEMP | 
| __IOM uint32_t | TEMPLIMITS | 
| __IOM uint32_t | VMONALTAVDDCTRL | 
| __IOM uint32_t | VMONAVDDCTRL | 
| __IOM uint32_t | VMONDVDDCTRL | 
| __IOM uint32_t | VMONIO0CTRL | 
Field Documentation
| __IOM uint32_t EMU_TypeDef::CMD | 
Command Register
        Definition at line
        
         54
        
        of file
        
         efr32bg14p_emu.h
        
        .
       
| __IOM uint32_t EMU_TypeDef::CTRL | 
Control Register
        Definition at line
        
         50
        
        of file
        
         efr32bg14p_emu.h
        
        .
       
| __IOM uint32_t EMU_TypeDef::DCDCCLIMCTRL | 
DCDC Power Train PFET Current Limiter Control Register
        Definition at line
        
         73
        
        of file
        
         efr32bg14p_emu.h
        
        .
       
| __IOM uint32_t EMU_TypeDef::DCDCCTRL | 
DCDC Control
        Definition at line
        
         68
        
        of file
        
         efr32bg14p_emu.h
        
        .
       
| __IOM uint32_t EMU_TypeDef::DCDCLNCOMPCTRL | 
DCDC Low Noise Compensator Control Register
        Definition at line
        
         74
        
        of file
        
         efr32bg14p_emu.h
        
        .
       
| __IOM uint32_t EMU_TypeDef::DCDCLNFREQCTRL | 
DCDC Low Noise Controller Frequency Control
        Definition at line
        
         82
        
        of file
        
         efr32bg14p_emu.h
        
        .
       
| __IOM uint32_t EMU_TypeDef::DCDCLNVCTRL | 
DCDC Low Noise Voltage Register
        Definition at line
        
         75
        
        of file
        
         efr32bg14p_emu.h
        
        .
       
| __IOM uint32_t EMU_TypeDef::DCDCLPCTRL | 
DCDC Low Power Control Register
        Definition at line
        
         81
        
        of file
        
         efr32bg14p_emu.h
        
        .
       
| __IOM uint32_t EMU_TypeDef::DCDCLPEM01CFG | 
Configuration Bits for Low Power Mode to Be Applied During EM01, This Field is Only Relevant If LP Mode is Used in EM01
        Definition at line
        
         98
        
        of file
        
         efr32bg14p_emu.h
        
        .
       
| __IOM uint32_t EMU_TypeDef::DCDCLPVCTRL | 
DCDC Low Power Voltage Register
        Definition at line
        
         78
        
        of file
        
         efr32bg14p_emu.h
        
        .
       
| __IOM uint32_t EMU_TypeDef::DCDCMISCCTRL | 
DCDC Miscellaneous Control Register
        Definition at line
        
         71
        
        of file
        
         efr32bg14p_emu.h
        
        .
       
| __IM uint32_t EMU_TypeDef::DCDCSYNC | 
DCDC Read Status Register
        Definition at line
        
         85
        
        of file
        
         efr32bg14p_emu.h
        
        .
       
| __IOM uint32_t EMU_TypeDef::DCDCZDETCTRL | 
DCDC Power Train NFET Zero Current Detector Control Register
        Definition at line
        
         72
        
        of file
        
         efr32bg14p_emu.h
        
        .
       
| __IOM uint32_t EMU_TypeDef::EM23PERNORETAINCMD | 
Clears Corresponding Bits in EM23PERNORETAINSTATUS Unlocking Access to Peripheral
        Definition at line
        
         101
        
        of file
        
         efr32bg14p_emu.h
        
        .
       
| __IOM uint32_t EMU_TypeDef::EM23PERNORETAINCTRL | 
When Set Corresponding Peripherals May Get Powered Down in EM23
        Definition at line
        
         103
        
        of file
        
         efr32bg14p_emu.h
        
        .
       
| __IM uint32_t EMU_TypeDef::EM23PERNORETAINSTATUS | 
Status Indicating If Peripherals Were Powered Down in EM23, Subsequently Locking Access to It
        Definition at line
        
         102
        
        of file
        
         efr32bg14p_emu.h
        
        .
       
| __IOM uint32_t EMU_TypeDef::EM4CTRL | 
EM4 Control Register
        Definition at line
        
         57
        
        of file
        
         efr32bg14p_emu.h
        
        .
       
| __IOM uint32_t EMU_TypeDef::IEN | 
Interrupt Enable Register
        Definition at line
        
         63
        
        of file
        
         efr32bg14p_emu.h
        
        .
       
| __IM uint32_t EMU_TypeDef::IF | 
Interrupt Flag Register
        Definition at line
        
         60
        
        of file
        
         efr32bg14p_emu.h
        
        .
       
| __IOM uint32_t EMU_TypeDef::IFC | 
Interrupt Flag Clear Register
        Definition at line
        
         62
        
        of file
        
         efr32bg14p_emu.h
        
        .
       
| __IOM uint32_t EMU_TypeDef::IFS | 
Interrupt Flag Set Register
        Definition at line
        
         61
        
        of file
        
         efr32bg14p_emu.h
        
        .
       
| __IOM uint32_t EMU_TypeDef::LOCK | 
Configuration Lock Register
        Definition at line
        
         52
        
        of file
        
         efr32bg14p_emu.h
        
        .
       
| __IOM uint32_t EMU_TypeDef::PWRCTRL | 
Power Control Register
        Definition at line
        
         67
        
        of file
        
         efr32bg14p_emu.h
        
        .
       
| __IOM uint32_t EMU_TypeDef::PWRLOCK | 
Regulator and Supply Lock Register
        Definition at line
        
         64
        
        of file
        
         efr32bg14p_emu.h
        
        .
       
| __IOM uint32_t EMU_TypeDef::RAM0CTRL | 
Memory Control Register
        Definition at line
        
         53
        
        of file
        
         efr32bg14p_emu.h
        
        .
       
| __IOM uint32_t EMU_TypeDef::RAM1CTRL | 
Memory Control Register
        Definition at line
        
         94
        
        of file
        
         efr32bg14p_emu.h
        
        .
       
| __IOM uint32_t EMU_TypeDef::RAM2CTRL | 
Memory Control Register
        Definition at line
        
         95
        
        of file
        
         efr32bg14p_emu.h
        
        .
       
| uint32_t EMU_TypeDef::RESERVED0[1] | 
Reserved for future use
        Definition at line
        
         56
        
        of file
        
         efr32bg14p_emu.h
        
        .
       
| uint32_t EMU_TypeDef::RESERVED1[1] | 
Reserved for future use
        Definition at line
        
         66
        
        of file
        
         efr32bg14p_emu.h
        
        .
       
| uint32_t EMU_TypeDef::RESERVED2[2] | 
Reserved for future use
        Definition at line
        
         70
        
        of file
        
         efr32bg14p_emu.h
        
        .
       
| uint32_t EMU_TypeDef::RESERVED3[1] | 
Reserved for future use
        Definition at line
        
         77
        
        of file
        
         efr32bg14p_emu.h
        
        .
       
| uint32_t EMU_TypeDef::RESERVED4[1] | 
Reserved for future use
        Definition at line
        
         80
        
        of file
        
         efr32bg14p_emu.h
        
        .
       
| uint32_t EMU_TypeDef::RESERVED5[1] | 
Reserved for future use
        Definition at line
        
         84
        
        of file
        
         efr32bg14p_emu.h
        
        .
       
| uint32_t EMU_TypeDef::RESERVED6[5] | 
Reserved for future use
        Definition at line
        
         87
        
        of file
        
         efr32bg14p_emu.h
        
        .
       
| uint32_t EMU_TypeDef::RESERVED7[5] | 
Reserved for future use
        Definition at line
        
         93
        
        of file
        
         efr32bg14p_emu.h
        
        .
       
| uint32_t EMU_TypeDef::RESERVED8[12] | 
Reserved for future use
        Definition at line
        
         97
        
        of file
        
         efr32bg14p_emu.h
        
        .
       
| uint32_t EMU_TypeDef::RESERVED9[4] | 
Reserved for future use
        Definition at line
        
         100
        
        of file
        
         efr32bg14p_emu.h
        
        .
       
| __IM uint32_t EMU_TypeDef::STATUS | 
Status Register
        Definition at line
        
         51
        
        of file
        
         efr32bg14p_emu.h
        
        .
       
| __IM uint32_t EMU_TypeDef::TEMP | 
Value of Last Temperature Measurement
        Definition at line
        
         59
        
        of file
        
         efr32bg14p_emu.h
        
        .
       
| __IOM uint32_t EMU_TypeDef::TEMPLIMITS | 
Temperature Limits for Interrupt Generation
        Definition at line
        
         58
        
        of file
        
         efr32bg14p_emu.h
        
        .
       
| __IOM uint32_t EMU_TypeDef::VMONALTAVDDCTRL | 
Alternate VMON AVDD Channel Control
        Definition at line
        
         89
        
        of file
        
         efr32bg14p_emu.h
        
        .
       
| __IOM uint32_t EMU_TypeDef::VMONAVDDCTRL | 
VMON AVDD Channel Control
        Definition at line
        
         88
        
        of file
        
         efr32bg14p_emu.h
        
        .
       
| __IOM uint32_t EMU_TypeDef::VMONDVDDCTRL | 
VMON DVDD Channel Control
        Definition at line
        
         90
        
        of file
        
         efr32bg14p_emu.h
        
        .
       
| __IOM uint32_t EMU_TypeDef::VMONIO0CTRL | 
VMON IOVDD0 Channel Control
        Definition at line
        
         91
        
        of file
        
         efr32bg14p_emu.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFR32BG14P/Include/
       
efr32bg14p_emu.h