ACMP_CapsenseInit_TypeDef Struct ReferenceEMLIB > ACMP
Capsense initialization structure.
       Definition at line
       
        525
       
       of file
       
        em_acmp.h
       
       .
      
      
       #include <
       
     
        em_acmp.h
       
       >
      
         Data Fields | 
       |
| uint32_t | biasProg | 
| bool | enable | 
| bool | fullBias | 
| ACMP_HysteresisLevel_TypeDef | hysteresisLevel_0 | 
| ACMP_HysteresisLevel_TypeDef | hysteresisLevel_1 | 
| ACMP_CapsenseResistor_TypeDef | resistor | 
| uint32_t | vddLevelHigh | 
| uint32_t | vddLevelLow | 
Field Documentation
| uint32_t ACMP_CapsenseInit_TypeDef::biasProg | 
Bias current. See the ACMP chapter about bias and response time in the reference manual for details.
        Definition at line
        
         538
        
        of file
        
         em_acmp.h
        
        .
       
Referenced by ACMP_CapsenseInit() .
| bool ACMP_CapsenseInit_TypeDef::enable | 
If true, ACMP is being enabled after configuration.
        Definition at line
        
         592
        
        of file
        
         em_acmp.h
        
        .
       
Referenced by ACMP_CapsenseInit() .
| bool ACMP_CapsenseInit_TypeDef::fullBias | 
Full bias current. See the ACMP chapter about bias and response time in the reference manual for details.
        Definition at line
        
         528
        
        of file
        
         em_acmp.h
        
        .
       
Referenced by ACMP_CapsenseInit() , and CAPLESENSE_setupACMP() .
| ACMP_HysteresisLevel_TypeDef ACMP_CapsenseInit_TypeDef::hysteresisLevel_0 | 
Hysteresis level when ACMP output is 0
        Definition at line
        
         551
        
        of file
        
         em_acmp.h
        
        .
       
Referenced by ACMP_CapsenseInit() .
| ACMP_HysteresisLevel_TypeDef ACMP_CapsenseInit_TypeDef::hysteresisLevel_1 | 
Hysteresis level when ACMP output is 1
        Definition at line
        
         554
        
        of file
        
         em_acmp.h
        
        .
       
Referenced by ACMP_CapsenseInit() .
| ACMP_CapsenseResistor_TypeDef ACMP_CapsenseInit_TypeDef::resistor | 
Resistor used in the capacative sensing circuit. For values see your device datasheet.
        Definition at line
        
         559
        
        of file
        
         em_acmp.h
        
        .
       
Referenced by ACMP_CapsenseInit() .
| uint32_t ACMP_CapsenseInit_TypeDef::vddLevelHigh | 
This value configures the upper voltage threshold of the capsense oscillation rail.
The voltage threshold is calculated as Vdd * (vddLevelHigh + 1) / 64
        Definition at line
        
         579
        
        of file
        
         em_acmp.h
        
        .
       
Referenced by ACMP_CapsenseInit() .
| uint32_t ACMP_CapsenseInit_TypeDef::vddLevelLow | 
This value configures the lower voltage threshold of the capsense oscillation rail.
The voltage threshold is calculated as Vdd * (vddLevelLow + 1) / 64
        Definition at line
        
         588
        
        of file
        
         em_acmp.h
        
        .
       
Referenced by ACMP_CapsenseInit() .
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/emlib/inc/
       
em_acmp.h