LDMA_TypeDef Struct ReferenceDevices > LDMA
LDMA Register Declaration
       Definition at line
       
        49
       
       of file
       
        efr32bg14p_ldma.h
       
       .
      
      
       #include <
       
     
        efr32bg14p_ldma.h
       
       >
      
         Data Fields | 
       |
| LDMA_CH_TypeDef | CH [8] | 
| __IM uint32_t | CHBUSY | 
| __IOM uint32_t | CHDONE | 
| __IOM uint32_t | CHEN | 
| __IOM uint32_t | CTRL | 
| __IOM uint32_t | DBGHALT | 
| __IOM uint32_t | IEN | 
| __IM uint32_t | IF | 
| __IOM uint32_t | IFC | 
| __IOM uint32_t | IFS | 
| __IOM uint32_t | LINKLOAD | 
| __IOM uint32_t | REQCLEAR | 
| __IOM uint32_t | REQDIS | 
| __IM uint32_t | REQPEND | 
| uint32_t | RESERVED0 [5] | 
| uint32_t | RESERVED1 [7] | 
| uint32_t | RESERVED2 [4] | 
| __IM uint32_t | STATUS | 
| __IOM uint32_t | SWREQ | 
| __IOM uint32_t | SYNC | 
Field Documentation
| LDMA_CH_TypeDef LDMA_TypeDef::CH[8] | 
DMA Channel Registers
        Definition at line
        
         70
        
        of file
        
         efr32bg14p_ldma.h
        
        .
       
| __IM uint32_t LDMA_TypeDef::CHBUSY | 
DMA Channel Busy Register
        Definition at line
        
         55
        
        of file
        
         efr32bg14p_ldma.h
        
        .
       
| __IOM uint32_t LDMA_TypeDef::CHDONE | 
DMA Channel Linking Done Register (Single-Cycle RMW)
        Definition at line
        
         56
        
        of file
        
         efr32bg14p_ldma.h
        
        .
       
| __IOM uint32_t LDMA_TypeDef::CHEN | 
DMA Channel Enable Register (Single-Cycle RMW)
        Definition at line
        
         54
        
        of file
        
         efr32bg14p_ldma.h
        
        .
       
| __IOM uint32_t LDMA_TypeDef::CTRL | 
DMA Control Register
        Definition at line
        
         50
        
        of file
        
         efr32bg14p_ldma.h
        
        .
       
| __IOM uint32_t LDMA_TypeDef::DBGHALT | 
DMA Channel Debug Halt Register
        Definition at line
        
         57
        
        of file
        
         efr32bg14p_ldma.h
        
        .
       
| __IOM uint32_t LDMA_TypeDef::IEN | 
Interrupt Enable Register
        Definition at line
        
         67
        
        of file
        
         efr32bg14p_ldma.h
        
        .
       
| __IM uint32_t LDMA_TypeDef::IF | 
Interrupt Flag Register
        Definition at line
        
         64
        
        of file
        
         efr32bg14p_ldma.h
        
        .
       
| __IOM uint32_t LDMA_TypeDef::IFC | 
Interrupt Flag Clear Register
        Definition at line
        
         66
        
        of file
        
         efr32bg14p_ldma.h
        
        .
       
| __IOM uint32_t LDMA_TypeDef::IFS | 
Interrupt Flag Set Register
        Definition at line
        
         65
        
        of file
        
         efr32bg14p_ldma.h
        
        .
       
| __IOM uint32_t LDMA_TypeDef::LINKLOAD | 
DMA Channel Link Load Register
        Definition at line
        
         61
        
        of file
        
         efr32bg14p_ldma.h
        
        .
       
| __IOM uint32_t LDMA_TypeDef::REQCLEAR | 
DMA Channel Request Clear Register
        Definition at line
        
         62
        
        of file
        
         efr32bg14p_ldma.h
        
        .
       
| __IOM uint32_t LDMA_TypeDef::REQDIS | 
DMA Channel Request Disable Register
        Definition at line
        
         59
        
        of file
        
         efr32bg14p_ldma.h
        
        .
       
| __IM uint32_t LDMA_TypeDef::REQPEND | 
DMA Channel Requests Pending Register
        Definition at line
        
         60
        
        of file
        
         efr32bg14p_ldma.h
        
        .
       
| uint32_t LDMA_TypeDef::RESERVED0[5] | 
Reserved for future use
        Definition at line
        
         53
        
        of file
        
         efr32bg14p_ldma.h
        
        .
       
| uint32_t LDMA_TypeDef::RESERVED1[7] | 
Reserved for future use
        Definition at line
        
         63
        
        of file
        
         efr32bg14p_ldma.h
        
        .
       
| uint32_t LDMA_TypeDef::RESERVED2[4] | 
Reserved registers
        Definition at line
        
         69
        
        of file
        
         efr32bg14p_ldma.h
        
        .
       
| __IM uint32_t LDMA_TypeDef::STATUS | 
DMA Status Register
        Definition at line
        
         51
        
        of file
        
         efr32bg14p_ldma.h
        
        .
       
| __IOM uint32_t LDMA_TypeDef::SWREQ | 
DMA Channel Software Transfer Request Register
        Definition at line
        
         58
        
        of file
        
         efr32bg14p_ldma.h
        
        .
       
| __IOM uint32_t LDMA_TypeDef::SYNC | 
DMA Synchronization Trigger Register (Single-Cycle RMW)
        Definition at line
        
         52
        
        of file
        
         efr32bg14p_ldma.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFR32BG14P/Include/
       
efr32bg14p_ldma.h