FPUEH_TypeDef Struct ReferenceDevices > FPUEH
FPUEH Register Declaration
       Definition at line
       
        49
       
       of file
       
        efr32bg14p_fpueh.h
       
       .
      
      
       #include <
       
     
        efr32bg14p_fpueh.h
       
       >
      
         Data Fields | 
       |
| __IOM uint32_t | IEN | 
| __IM uint32_t | IF | 
| __IOM uint32_t | IFC | 
| __IOM uint32_t | IFS | 
Field Documentation
| __IOM uint32_t FPUEH_TypeDef::IEN | 
Interrupt Enable Register
        Definition at line
        
         53
        
        of file
        
         efr32bg14p_fpueh.h
        
        .
       
| __IM uint32_t FPUEH_TypeDef::IF | 
Interrupt Flag Register
        Definition at line
        
         50
        
        of file
        
         efr32bg14p_fpueh.h
        
        .
       
| __IOM uint32_t FPUEH_TypeDef::IFC | 
Interrupt Flag Clear Register
        Definition at line
        
         52
        
        of file
        
         efr32bg14p_fpueh.h
        
        .
       
| __IOM uint32_t FPUEH_TypeDef::IFS | 
Interrupt Flag Set Register
        Definition at line
        
         51
        
        of file
        
         efr32bg14p_fpueh.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFR32BG14P/Include/
       
efr32bg14p_fpueh.h