ROMTABLE_TypeDef Struct ReferenceDevices > ROM Table, Chip Revision Information
ROMTABLE Register Declaration
       Definition at line
       
        49
       
       of file
       
        efr32bg14p_romtable.h
       
       .
      
      
       #include <
       
     
        efr32bg14p_romtable.h
       
       >
      
         Data Fields | 
       |
| __IM uint32_t | CID0 | 
| __IM uint32_t | PID0 | 
| __IM uint32_t | PID1 | 
| __IM uint32_t | PID2 | 
| __IM uint32_t | PID3 | 
| __IM uint32_t | PID4 | 
| __IM uint32_t | PID5 | 
| __IM uint32_t | PID6 | 
| __IM uint32_t | PID7 | 
Field Documentation
| __IM uint32_t ROMTABLE_TypeDef::CID0 | 
Unused
        Definition at line
        
         58
        
        of file
        
         efr32bg14p_romtable.h
        
        .
       
| __IM uint32_t ROMTABLE_TypeDef::PID0 | 
Chip family LSB, chip major revision
        Definition at line
        
         54
        
        of file
        
         efr32bg14p_romtable.h
        
        .
       
| __IM uint32_t ROMTABLE_TypeDef::PID1 | 
JEP_106_NO, Chip family MSB
        Definition at line
        
         55
        
        of file
        
         efr32bg14p_romtable.h
        
        .
       
| __IM uint32_t ROMTABLE_TypeDef::PID2 | 
Chip minor rev MSB, JEP_106_PRESENT, JEP_106_NO
        Definition at line
        
         56
        
        of file
        
         efr32bg14p_romtable.h
        
        .
       
| __IM uint32_t ROMTABLE_TypeDef::PID3 | 
Chip minor rev LSB
        Definition at line
        
         57
        
        of file
        
         efr32bg14p_romtable.h
        
        .
       
| __IM uint32_t ROMTABLE_TypeDef::PID4 | 
JEP_106_BANK
        Definition at line
        
         50
        
        of file
        
         efr32bg14p_romtable.h
        
        .
       
| __IM uint32_t ROMTABLE_TypeDef::PID5 | 
Unused
        Definition at line
        
         51
        
        of file
        
         efr32bg14p_romtable.h
        
        .
       
| __IM uint32_t ROMTABLE_TypeDef::PID6 | 
Unused
        Definition at line
        
         52
        
        of file
        
         efr32bg14p_romtable.h
        
        .
       
| __IM uint32_t ROMTABLE_TypeDef::PID7 | 
Unused
        Definition at line
        
         53
        
        of file
        
         efr32bg14p_romtable.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFR32BG14P/Include/
       
efr32bg14p_romtable.h