OPAMP_Init_TypeDef Struct ReferenceEMLIB > OPAMP
OPAMP init structure.
       Definition at line
       
        437
       
       of file
       
        em_opamp.h
       
       .
      
      
       #include <
       
     
        em_opamp.h
       
       >
      
         Data Fields | 
       |
| bool | aportXMasterDisable | 
| bool | aportYMasterDisable | 
| bool | defaultOffsetN | 
| bool | defaultOffsetP | 
| OPAMP_DrvStr_Typedef | drvStr | 
| bool | gain3xEn | 
| bool | halfDrvStr | 
| bool | hcmDisable | 
| OPAMP_NegSel_TypeDef | negSel | 
| uint32_t | offsetN | 
| uint32_t | offsetP | 
| OPAMP_OutMode_TypeDef | outMode | 
| uint32_t | outPen | 
| OPAMP_PosSel_TypeDef | posSel | 
| bool | prsEn | 
| OPAMP_PrsMode_TypeDef | prsMode | 
| OPAMP_PrsOut_TypeDef | prsOutSel | 
| OPAMP_PrsSel_TypeDef | prsSel | 
| OPAMP_ResInMux_TypeDef | resInMux | 
| OPAMP_ResSel_TypeDef | resSel | 
| uint32_t | settleTime | 
| uint32_t | startupDly | 
| bool | ugBwScale | 
Field Documentation
| bool OPAMP_Init_TypeDef::aportXMasterDisable | 
Disable bus master request on APORT X.
        Definition at line
        
         510
        
        of file
        
         em_opamp.h
        
        .
       
Referenced by OPAMP_Enable() .
| bool OPAMP_Init_TypeDef::aportYMasterDisable | 
Disable bus master request on APORT Y.
        Definition at line
        
         509
        
        of file
        
         em_opamp.h
        
        .
       
Referenced by OPAMP_Enable() .
| bool OPAMP_Init_TypeDef::defaultOffsetN | 
Use factory calibrated opamp inverting input offset value.
        Definition at line
        
         514
        
        of file
        
         em_opamp.h
        
        .
       
Referenced by OPAMP_Enable() .
| bool OPAMP_Init_TypeDef::defaultOffsetP | 
Use factory calibrated opamp non-inverting input offset value.
        Definition at line
        
         518
        
        of file
        
         em_opamp.h
        
        .
       
Referenced by OPAMP_Enable() .
| OPAMP_DrvStr_Typedef OPAMP_Init_TypeDef::drvStr | 
| bool OPAMP_Init_TypeDef::gain3xEn | 
Enable 3x gain resistor ladder.
        Definition at line
        
         502
        
        of file
        
         em_opamp.h
        
        .
       
Referenced by OPAMP_Enable() .
| bool OPAMP_Init_TypeDef::halfDrvStr | 
Half or full output drive strength.
        Definition at line
        
         503
        
        of file
        
         em_opamp.h
        
        .
       
Referenced by OPAMP_Enable() .
| bool OPAMP_Init_TypeDef::hcmDisable | 
Disable input rail-to-rail capability.
        Definition at line
        
         513
        
        of file
        
         em_opamp.h
        
        .
       
Referenced by OPAMP_Enable() .
| OPAMP_NegSel_TypeDef OPAMP_Init_TypeDef::negSel | 
Select input source for negative terminal.
        Definition at line
        
         438
        
        of file
        
         em_opamp.h
        
        .
       
Referenced by OPAMP_Enable() .
| uint32_t OPAMP_Init_TypeDef::offsetN | 
Opamp inverting input offset value when defaultOffsetInv is false.
        Definition at line
        
         516
        
        of file
        
         em_opamp.h
        
        .
       
Referenced by OPAMP_Enable() .
| uint32_t OPAMP_Init_TypeDef::offsetP | 
Opamp non-inverting input offset value when defaultOffsetNon is false.
        Definition at line
        
         520
        
        of file
        
         em_opamp.h
        
        .
       
Referenced by OPAMP_Enable() .
| OPAMP_OutMode_TypeDef OPAMP_Init_TypeDef::outMode | 
Output terminal connection.
        Definition at line
        
         440
        
        of file
        
         em_opamp.h
        
        .
       
Referenced by OPAMP_Enable() .
| uint32_t OPAMP_Init_TypeDef::outPen | 
        Alternate output enable bit mask. This value should consist of one or more of the VDAC_OPA_OUT_ALTOUTPADEN_OUT[output#] flags (defined in <part_name>_vdac.h) OR'ed together.
        
        
       
- VDAC_OPA_OUT_ALTOUTPADEN_OUT0
 - VDAC_OPA_OUT_ALTOUTPADEN_OUT1
 - VDAC_OPA_OUT_ALTOUTPADEN_OUT2
 - VDAC_OPA_OUT_ALTOUTPADEN_OUT3
 - VDAC_OPA_OUT_ALTOUTPADEN_OUT4
 
        E.g:
        
        init.outPen = VDAC_OPA_OUT_ALTOUTPADEN_OUT0 | VDAC_OPA_OUT_ALTOUTPADEN_OUT2 | VDAC_OPA_OUT_ALTOUTPADEN_OUT4;
       
        Definition at line
        
         443
        
        of file
        
         em_opamp.h
        
        .
       
Referenced by OPAMP_Enable() .
| OPAMP_PosSel_TypeDef OPAMP_Init_TypeDef::posSel | 
Select input source for positive terminal.
        Definition at line
        
         439
        
        of file
        
         em_opamp.h
        
        .
       
Referenced by OPAMP_Enable() .
| bool OPAMP_Init_TypeDef::prsEn | 
Enable PRS as OPAMP trigger.
        Definition at line
        
         505
        
        of file
        
         em_opamp.h
        
        .
       
Referenced by OPAMP_Enable() .
| OPAMP_PrsMode_TypeDef OPAMP_Init_TypeDef::prsMode | 
Selects PRS trigger mode.
        Definition at line
        
         506
        
        of file
        
         em_opamp.h
        
        .
       
Referenced by OPAMP_Enable() .
| OPAMP_PrsOut_TypeDef OPAMP_Init_TypeDef::prsOutSel | 
| OPAMP_PrsSel_TypeDef OPAMP_Init_TypeDef::prsSel | 
PRS channel trigger select.
        Definition at line
        
         507
        
        of file
        
         em_opamp.h
        
        .
       
Referenced by OPAMP_Enable() .
| OPAMP_ResInMux_TypeDef OPAMP_Init_TypeDef::resInMux | 
Select input source for resistor ladder.
        Definition at line
        
         442
        
        of file
        
         em_opamp.h
        
        .
       
Referenced by OPAMP_Enable() .
| OPAMP_ResSel_TypeDef OPAMP_Init_TypeDef::resSel | 
Select R2/R1 resistor ratio.
        Definition at line
        
         441
        
        of file
        
         em_opamp.h
        
        .
       
Referenced by OPAMP_Enable() .
| uint32_t OPAMP_Init_TypeDef::settleTime | 
Number of clock cycles to drive the output.
        Definition at line
        
         511
        
        of file
        
         em_opamp.h
        
        .
       
Referenced by OPAMP_Enable() .
| uint32_t OPAMP_Init_TypeDef::startupDly | 
OPAx startup delay in us.
        Definition at line
        
         512
        
        of file
        
         em_opamp.h
        
        .
       
Referenced by OPAMP_Enable() .
| bool OPAMP_Init_TypeDef::ugBwScale | 
Unity gain bandwidth scaled by factor of 2.5.
        Definition at line
        
         504
        
        of file
        
         em_opamp.h
        
        .
       
Referenced by OPAMP_Enable() .
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/emlib/inc/
       
em_opamp.h