LESENSE_CoreCtrlDesc_TypeDef Struct ReferenceEMLIB > LESENSE
Core control (LESENSE_CTRL) descriptor structure.
       Definition at line
       
        490
       
       of file
       
        em_lesense.h
       
       .
      
      
       #include <
       
     
        em_lesense.h
       
       >
      
Field Documentation
| LESENSE_BiasMode_TypeDef LESENSE_CoreCtrlDesc_TypeDef::biasMode | 
| bool LESENSE_CoreCtrlDesc_TypeDef::bufOverWr | 
Set to true in order to always make LESENSE write to the result buffer, even if it is full.
        Definition at line
        
         515
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
| LESENSE_BufTrigLevel_TypeDef LESENSE_CoreCtrlDesc_TypeDef::bufTrigLevel | 
Select trigger conditions for interrupt and DMA.
        Definition at line
        
         518
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
| bool LESENSE_CoreCtrlDesc_TypeDef::debugRun | 
Set to true to keep LESENSE running in debug mode.
        Definition at line
        
         527
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
| bool LESENSE_CoreCtrlDesc_TypeDef::dualSample | 
Set to true to sample both ACMPs simultaneously.
        Definition at line
        
         507
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
| bool LESENSE_CoreCtrlDesc_TypeDef::invACMP0 | 
Set to true to invert ACMP0 output.
        Definition at line
        
         501
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
| bool LESENSE_CoreCtrlDesc_TypeDef::invACMP1 | 
Set to true to invert ACMP1 output.
        Definition at line
        
         504
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
| LESENSE_PRSSel_TypeDef LESENSE_CoreCtrlDesc_TypeDef::prsSel | 
Select PRS source for scan start if scanMode is set to lesensePrsPulse.
        Definition at line
        
         495
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
| LESENSE_ScanConfSel_TypeDef LESENSE_CoreCtrlDesc_TypeDef::scanConfSel | 
Select scan configuration register usage strategy.
        Definition at line
        
         498
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
| LESENSE_ScanMode_TypeDef LESENSE_CoreCtrlDesc_TypeDef::scanStart | 
Select scan start mode to control how the scan start is being triggered.
        Definition at line
        
         492
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by CAPLESENSE_setupLESENSE() , and LESENSE_Init() .
| bool LESENSE_CoreCtrlDesc_TypeDef::storeScanRes | 
Set to true in order to to store SCANRES in RAM (accessible via RESDATA) after each scan.
        Definition at line
        
         511
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
| LESENSE_DMAWakeUp_TypeDef LESENSE_CoreCtrlDesc_TypeDef::wakeupOnDMA | 
Configure trigger condition for DMA wakeup from EM2.
        Definition at line
        
         521
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/emlib/inc/
       
em_lesense.h