TftKit Drivers
         Functions | 
       |
| void | SPI_TFT_Init (void) | 
| 
         SPI_TFT_Init Initialize SPI interface to TFT-LCD SSD2119 controller.
          | 
       |
| void | SPI_TFT_WriteRegister (uint8_t reg, uint16_t data) | 
| 
         SPI_TFT_Write Write registers/data to SSD2119 controller.
          | 
       |
| bool | TFT_AddressMappedInit (void) | 
| 
         TFT initialize or reinitialize to Address Mapped Mode Assumes EBI has been configured correctly in BSP_Init(BSP_INIT_DK_EBI)
          | 
       |
| void | TFT_DirectGPIOConfig (void) | 
| 
         GPIO configuration for TFT direct drive.
          | 
       |
| bool | TFT_DirectInit (const EBI_TFTInit_TypeDef *tftInit) | 
| 
         TFT initialize or reinitialize Assumes EBI has been configured correctly in BSP_Init(BSP_INIT_DK_EBI)
          | 
       |
Function Documentation
| void SPI_TFT_Init | ( | void | 
           
           
           | 
          ) | 
SPI_TFT_Init Initialize SPI interface to TFT-LCD SSD2119 controller.
- Note
 - To enable access, be sure to call the functions BSP_PeripheralAccess(BSP_TFT, enable); before using this interface.
 
        Definition at line
        
         43
        
        of file
        
         tftspi.c
        
        .
       
References CMU_ClockEnable() , cmuClock_GPIO , cmuClock_HFPER , cmuClock_USART1 , GPIO_PinModeSet() , gpioModeInput , gpioModePushPull , USART1 , USART_InitSync() , and USART_Reset() .
| void SPI_TFT_WriteRegister | ( | uint8_t | 
           
            reg,
           
           | 
         
| uint16_t | 
           
            data
           
           | 
         ||
| ) | 
SPI_TFT_Write Write registers/data to SSD2119 controller.
- Parameters
 - 
         
regRegister to write to data16-bit data to write into register  
- Note
 - It's not possible to read back register value through SSD2119 SPI interface, so no SPI_TFT_ReadRegister function is implemented
 
        Definition at line
        
         78
        
        of file
        
         tftspi.c
        
        .
       
References GPIO_PinOutClear() , GPIO_PinOutSet() , USART1 , USART_CTRL_BIT8DV , USART_Rx() , and USART_Tx() .
| bool TFT_AddressMappedInit | ( | void | 
           
           
           | 
          ) | 
TFT initialize or reinitialize to Address Mapped Mode Assumes EBI has been configured correctly in BSP_Init(BSP_INIT_DK_EBI)
- Returns
 - true if we should redraw into buffer, false if BC has control over display
 
        Definition at line
        
         36
        
        of file
        
         tftamapped.c
        
        .
       
References BC_ARB_CTRL_EBI , BC_REGISTER , BC_SPI_DEMUX_SLAVE_AUDIO , BC_SPI_DEMUX_SLAVE_DISPLAY , BC_SSD2119_BASE , BC_UIF_AEM_EFM , BSP_Display_EBI , BSP_Display_Mode8080 , BSP_Display_PowerDisable , BSP_Display_PowerEnable , BSP_Display_ResetAssert , BSP_Display_ResetRelease , BSP_DisplayControl() , BSP_RegisterRead() , BSP_RegisterWrite() , runOnce , and SystemCoreClockGet() .
| bool TFT_DirectInit | ( | const EBI_TFTInit_TypeDef * | 
           
            tftInit
           
           | 
          ) | 
TFT initialize or reinitialize Assumes EBI has been configured correctly in BSP_Init(BSP_INIT_DK_EBI)
- Parameters
 - 
         
[in] tftInitPointer to EBI TFT initialization structure  
- Returns
 - true if we should redraw into buffer, false if BC has control over display
 
        Definition at line
        
         52
        
        of file
        
         tftdirect.c
        
        .
       
References BC_ARB_CTRL_EBI , BC_REGISTER , BC_UIF_AEM_EFM , BSP_Display_EBI , BSP_Display_ModeGeneric , BSP_Display_PowerDisable , BSP_Display_PowerEnable , BSP_Display_ResetAssert , BSP_Display_ResetRelease , BSP_DisplayControl() , BSP_PeripheralAccess() , BSP_RegisterRead() , BSP_TFT , runOnce , SystemCoreClockGet() , and TFT_DirectGPIOConfig() .