spidrv.h File Reference
SPIDRV API definition.
- Version
 - 5.4.0
 
License
(C) Copyright 2014 Silicon Labs, www.silabs.com
This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.
       Definition in file
       
        spidrv.h
       
       .
      
       #include "
       
        em_device.h
       
       "
      
      
       #include "
       
        em_cmu.h
       
       "
      
      
       #include "
       
        ecode.h
       
       "
      
      
       #include "spidrv_config.h"
      
      
       #include "
       
        rtcdriver.h
       
       "
      
      
       #include "
       
        dmadrv.h
       
       "
      
      
         Data Structures | 
       |
| struct | SPIDRV_HandleData | 
| struct | SPIDRV_Init | 
         Macros | 
       |
| #define | ECODE_EMDRV_SPIDRV_ABORTED ( ECODE_EMDRV_SPIDRV_BASE | 0x00000007) | 
| 
         An SPI transfer has been aborted.
          | 
       |
| #define | ECODE_EMDRV_SPIDRV_BUSY ( ECODE_EMDRV_SPIDRV_BASE | 0x00000003) | 
| 
         The SPI port is busy.
          | 
       |
| #define | ECODE_EMDRV_SPIDRV_DMA_ALLOC_ERROR ( ECODE_EMDRV_SPIDRV_BASE | 0x00000009) | 
| 
         Unable to allocate DMA channels.
          | 
       |
| #define | ECODE_EMDRV_SPIDRV_IDLE ( ECODE_EMDRV_SPIDRV_BASE | 0x00000006) | 
| 
         No SPI transfer in progress.
          | 
       |
| #define | ECODE_EMDRV_SPIDRV_ILLEGAL_HANDLE ( ECODE_EMDRV_SPIDRV_BASE | 0x00000001) | 
| 
         An illegal SPI handle.
          | 
       |
| #define | ECODE_EMDRV_SPIDRV_MODE_ERROR ( ECODE_EMDRV_SPIDRV_BASE | 0x00000008) | 
| 
         SPI master used slave API or vica versa.
          | 
       |
| #define | ECODE_EMDRV_SPIDRV_OK ( ECODE_OK ) | 
| 
         A successful return value.
          | 
       |
| #define | ECODE_EMDRV_SPIDRV_PARAM_ERROR ( ECODE_EMDRV_SPIDRV_BASE | 0x00000002) | 
| 
         An illegal input parameter.
          | 
       |
| #define | ECODE_EMDRV_SPIDRV_TIMEOUT ( ECODE_EMDRV_SPIDRV_BASE | 0x00000005) | 
| 
         An SPI transfer timeout.
          | 
       |
| #define | ECODE_EMDRV_SPIDRV_TIMER_ALLOC_ERROR ( ECODE_EMDRV_SPIDRV_BASE | 0x00000004) | 
| 
         Unable to allocate timeout timer.
          | 
       |
| #define | SPIDRV_MASTER_USART0 | 
| 
         Configuration data for SPI master using USART0.
          | 
       |
| #define | SPIDRV_MASTER_USART1 | 
| 
         Configuration data for SPI master using USART1.
          | 
       |
| #define | SPIDRV_SLAVE_USART0 | 
| 
         Configuration data for SPI slave using USART0.
          | 
       |
| #define | SPIDRV_SLAVE_USART1 | 
| 
         Configuration data for SPI slave using USART1.
          | 
       |
         Typedefs | 
       |
| typedef enum SPIDRV_BitOrder | SPIDRV_BitOrder_t | 
| 
         SPI bus bit order.
          | 
       |
| typedef void(* | SPIDRV_Callback_t ) (struct SPIDRV_HandleData *handle, Ecode_t transferStatus, int itemsTransferred) | 
| 
         SPIDRV transfer completion callback function.
          | 
       |
| typedef enum SPIDRV_ClockMode | SPIDRV_ClockMode_t | 
| 
         SPI clock mode (clock polarity and phase).
          | 
       |
| typedef enum SPIDRV_CsControl | SPIDRV_CsControl_t | 
| 
         SPI master chip select (CS) control scheme.
          | 
       |
| typedef SPIDRV_HandleData_t * | SPIDRV_Handle_t | 
| 
         An SPI driver instance handle.
          | 
       |
| typedef struct SPIDRV_HandleData | SPIDRV_HandleData_t | 
| typedef struct SPIDRV_Init | SPIDRV_Init_t | 
| typedef enum SPIDRV_SlaveStart | SPIDRV_SlaveStart_t | 
| 
         SPI slave transfer start scheme.
          | 
       |
| typedef enum SPIDRV_Type | SPIDRV_Type_t | 
| 
         SPI driver instance type.
          | 
       |
         Enumerations | 
       |
| enum | 
         
          SPIDRV_BitOrder
         
         {
          spidrvBitOrderLsbFirst = 0, spidrvBitOrderMsbFirst = 1 }  | 
       
| 
         SPI bus bit order.
          | 
       |
| enum | 
         
          SPIDRV_ClockMode
         
         {
          spidrvClockMode0 = 0, spidrvClockMode1 = 1, spidrvClockMode2 = 2, spidrvClockMode3 = 3 }  | 
       
| 
         SPI clock mode (clock polarity and phase).
          | 
       |
| enum | 
         
          SPIDRV_CsControl
         
         {
          spidrvCsControlAuto = 0, spidrvCsControlApplication = 1 }  | 
       
| 
         SPI master chip select (CS) control scheme.
          | 
       |
| enum | 
         
          SPIDRV_SlaveStart
         
         {
          spidrvSlaveStartImmediate = 0, spidrvSlaveStartDelayed = 1 }  | 
       
| 
         SPI slave transfer start scheme.
          | 
       |
| enum | 
         
          SPIDRV_Type
         
         {
          spidrvMaster = 0, spidrvSlave = 1 }  | 
       
| 
         SPI driver instance type.
          | 
       |
         Functions | 
       |
| Ecode_t | SPIDRV_AbortTransfer ( SPIDRV_Handle_t handle) | 
| 
         Abort an ongoing SPI transfer.
          | 
       |
| Ecode_t | SPIDRV_DeInit ( SPIDRV_Handle_t handle) | 
| 
         Deinitialize an SPI driver instance.
          | 
       |
| Ecode_t | SPIDRV_GetBitrate ( SPIDRV_Handle_t handle, uint32_t *bitRate) | 
| 
         Get current SPI bus bitrate.
          | 
       |
| Ecode_t | SPIDRV_GetFramelength ( SPIDRV_Handle_t handle, uint32_t *frameLength) | 
| 
         Get current SPI framelength.
          | 
       |
| Ecode_t | SPIDRV_GetTransferStatus ( SPIDRV_Handle_t handle, int *itemsTransferred, int *itemsRemaining) | 
| 
         Get the status of an SPI transfer.
          | 
       |
| Ecode_t | SPIDRV_Init ( SPIDRV_Handle_t handle, SPIDRV_Init_t *initData) | 
| 
         Initialize an SPI driver instance.
          | 
       |
| Ecode_t | SPIDRV_MReceive ( SPIDRV_Handle_t handle, void *buffer, int count, SPIDRV_Callback_t callback) | 
| 
         Start an SPI master receive transfer.
          | 
       |
| Ecode_t | SPIDRV_MReceiveB ( SPIDRV_Handle_t handle, void *buffer, int count) | 
| 
         Start an SPI master blocking receive transfer.
          | 
       |
| Ecode_t | SPIDRV_MTransfer ( SPIDRV_Handle_t handle, const void *txBuffer, void * rxBuffer , int count, SPIDRV_Callback_t callback) | 
| 
         Start an SPI master transfer.
          | 
       |
| Ecode_t | SPIDRV_MTransferB ( SPIDRV_Handle_t handle, const void *txBuffer, void * rxBuffer , int count) | 
| 
         Start an SPI master blocking transfer.
          | 
       |
| Ecode_t | SPIDRV_MTransferSingleItemB ( SPIDRV_Handle_t handle, uint32_t txValue, void *rxValue) | 
| 
         Start an SPI master blocking single item (frame) transfer.
          | 
       |
| Ecode_t | SPIDRV_MTransmit ( SPIDRV_Handle_t handle, const void *buffer, int count, SPIDRV_Callback_t callback) | 
| 
         Start an SPI master transmit transfer.
          | 
       |
| Ecode_t | SPIDRV_MTransmitB ( SPIDRV_Handle_t handle, const void *buffer, int count) | 
| 
         Start an SPI master blocking transmit transfer.
          | 
       |
| Ecode_t | SPIDRV_SetBitrate ( SPIDRV_Handle_t handle, uint32_t bitRate) | 
| 
         Set SPI bus bitrate.
          | 
       |
| Ecode_t | SPIDRV_SetFramelength ( SPIDRV_Handle_t handle, uint32_t frameLength) | 
| 
         Set SPI framelength.
          | 
       |
| Ecode_t | SPIDRV_SReceive ( SPIDRV_Handle_t handle, void *buffer, int count, SPIDRV_Callback_t callback, int timeoutMs) | 
| 
         Start an SPI slave receive transfer.
          | 
       |
| Ecode_t | SPIDRV_SReceiveB ( SPIDRV_Handle_t handle, void *buffer, int count, int timeoutMs) | 
| 
         Start an SPI slave blocking receive transfer.
          | 
       |
| Ecode_t | SPIDRV_STransfer ( SPIDRV_Handle_t handle, const void *txBuffer, void * rxBuffer , int count, SPIDRV_Callback_t callback, int timeoutMs) | 
| 
         Start an SPI slave transfer.
          | 
       |
| Ecode_t | SPIDRV_STransferB ( SPIDRV_Handle_t handle, const void *txBuffer, void * rxBuffer , int count, int timeoutMs) | 
| 
         Start an SPI slave blocking transfer.
          | 
       |
| Ecode_t | SPIDRV_STransmit ( SPIDRV_Handle_t handle, const void *buffer, int count, SPIDRV_Callback_t callback, int timeoutMs) | 
| 
         Start an SPI slave transmit transfer.
          | 
       |
| Ecode_t | SPIDRV_STransmitB ( SPIDRV_Handle_t handle, const void *buffer, int count, int timeoutMs) | 
| 
         Start an SPI slave blocking transmit transfer.
          | 
       |