eeprom.c File Reference
EEPROM driver for 24AA024 (2Kbit) EEPROM device on the DK.
- Version
- 5.6.0
License
Copyright 2015 Silicon Labs, Inc. http://www.silabs.com
This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.
Definition in file
eeprom.c
.
#include <stddef.h>
#include "
i2cspm.h
"
#include "
eeprom.h
"
Macros |
|
| #define | EEPROM_DVK_LEN 0x100 |
| #define | EEPROM_DVK_PAGESIZE 16 |
Functions |
|
| static int | EEPROM_AckPoll ( I2C_TypeDef *i2c, uint8_t addr) |
|
Do acknowledge polling on EEPROM device.
|
|
| int | EEPROM_Read ( I2C_TypeDef *i2c, uint8_t addr, unsigned int offset, uint8_t *data, unsigned int len) |
|
Read data from EEPROM.
|
|
| int | EEPROM_Write ( I2C_TypeDef *i2c, uint8_t addr, unsigned int offset, uint8_t *data, unsigned int len) |
|
Write data to EEPROM.
|
|
Macro Definition Documentation
| #define EEPROM_DVK_LEN 0x100 |
Number of bytes in EEPROM
Definition at line
25
of file
eeprom.c
.
Referenced by EEPROM_Read() , and EEPROM_Write() .
| #define EEPROM_DVK_PAGESIZE 16 |
Function Documentation
|
static |
Do acknowledge polling on EEPROM device.
When writing to an EEPROM, the EEPROM device will be busy for some time after issuing a (page) write. During this time, the EEPROM is not accessible, and will therefore not ACK any requests. This feature can be used to determine when the write is actually completed, and is denoted acknowledgement polling.
- Note
- This function will not return until the EEPROM device acknowledges (or some sort of I2C failure occurs). If trying to acknowledge poll a non-existing device, NACK will always result and this function will never return. Thus, it should not be used unless the EEPROM device is actually present.
- Parameters
-
[in] i2cPointer to I2C peripheral register block. [in] addrI2C address for EEPROM, in 8 bit format, where LSB is reserved for R/W bit.
- Returns
- Returns 0 when EEPROM acknowledges. Negative value is returned is some sort of error occurred during acknowledgement polling.
Definition at line
62
of file
eeprom.c
.
References I2C_TransferSeq_TypeDef::addr , I2C_TransferSeq_TypeDef::buf , I2C_TransferSeq_TypeDef::data , I2C_TransferSeq_TypeDef::flags , I2C_FLAG_WRITE , I2CSPM_Transfer() , i2cTransferDone , i2cTransferNack , and I2C_TransferSeq_TypeDef::len .
Referenced by EEPROM_Write() .