LCD

Detailed Description

Liquid Crystal Display (LCD) Peripheral API.

This module contains functions to control the LDC peripheral of Silicon Labs 32-bit MCUs and SoCs. The LCD driver can drive up to 8x36 segmented LCD directly. The animation feature makes it possible to have active animations without the CPU intervention.

Data Structures

struct  LCD_AnimInit_TypeDef
 
struct  LCD_FrameCountInit_TypeDef
 
struct  LCD_Init_TypeDef
 

Macros

#define LCD_DEFAULT_CONTRAST   15
 
#define LCD_DEFAULT_FRAME_RATE_DIV   4
 
#define LCD_INIT_DEFAULT
 

Enumerations

enum  LCD_AnimLogic_TypeDef {
  lcdAnimLogicAnd = LCD_BACTRL_ALOGSEL_AND,
  lcdAnimLogicOr = LCD_BACTRL_ALOGSEL_OR
}
 
enum  LCD_AnimShift_TypeDef {
  lcdAnimShiftNone = _LCD_BACTRL_AREGASC_NOSHIFT,
  lcdAnimShiftLeft = _LCD_BACTRL_AREGASC_SHIFTLEFT,
  lcdAnimShiftRight = _LCD_BACTRL_AREGASC_SHIFTRIGHT
}
 
enum  LCD_Bias_TypeDef {
  lcdBiasStatic = LCD_DISPCTRL_BIAS_STATIC,
  lcdBiasOneHalf = LCD_DISPCTRL_BIAS_ONEHALF,
  lcdBiasOneThird = LCD_DISPCTRL_BIAS_ONETHIRD,
  lcdBiasOneFourth = LCD_DISPCTRL_BIAS_ONEFOURTH
}
 
enum  LCD_ConConf_TypeDef {
  lcdConConfVLCD = LCD_DISPCTRL_CONCONF_VLCD,
  lcdConConfGND = LCD_DISPCTRL_CONCONF_GND
}
 
enum  LCD_FCPreScale_TypeDef {
  lcdFCPrescDiv1 = LCD_BACTRL_FCPRESC_DIV1,
  lcdFCPrescDiv2 = LCD_BACTRL_FCPRESC_DIV2,
  lcdFCPrescDiv4 = LCD_BACTRL_FCPRESC_DIV4,
  lcdFCPrescDiv8 = LCD_BACTRL_FCPRESC_DIV8
}
 
enum  LCD_Mux_TypeDef {
  lcdMuxStatic = LCD_DISPCTRL_MUX_STATIC,
  lcdMuxDuplex = LCD_DISPCTRL_MUX_DUPLEX,
  lcdMuxTriplex = LCD_DISPCTRL_MUX_TRIPLEX,
  lcdMuxQuadruplex = LCD_DISPCTRL_MUX_QUADRUPLEX,
  lcdMuxSextaplex = LCD_DISPCTRL_MUXE_MUXE | LCD_DISPCTRL_MUX_DUPLEX,
  lcdMuxOctaplex = LCD_DISPCTRL_MUXE_MUXE | LCD_DISPCTRL_MUX_QUADRUPLEX
}
 
enum  LCD_SegmentRange_TypeDef {
  lcdSegment0_3 = (1 << 0),
  lcdSegment4_7 = (1 << 1),
  lcdSegment8_11 = (1 << 2),
  lcdSegment12_15 = (1 << 3),
  lcdSegment16_19 = (1 << 4),
  lcdSegment20_23 = (1 << 5),
  lcdSegment24_27 = (1 << 6),
  lcdSegment28_31 = (1 << 7),
  lcdSegment32_35 = (1 << 8),
  lcdSegment36_39 = (1 << 9),
  lcdSegmentAll = (0x03ff)
}
 
enum  LCD_UpdateCtrl_TypeDef {
  lcdUpdateCtrlRegular = LCD_CTRL_UDCTRL_REGULAR,
  lcdUpdateCtrlFCEvent = LCD_CTRL_UDCTRL_FCEVENT,
  lcdUpdateCtrlFrameStart = LCD_CTRL_UDCTRL_FRAMESTART
}
 
enum  LCD_VBoostLevel_TypeDef {
  lcdVBoostLevel0 = LCD_DISPCTRL_VBLEV_LEVEL0,
  lcdVBoostLevel1 = LCD_DISPCTRL_VBLEV_LEVEL1,
  lcdVBoostLevel2 = LCD_DISPCTRL_VBLEV_LEVEL2,
  lcdVBoostLevel3 = LCD_DISPCTRL_VBLEV_LEVEL3,
  lcdVBoostLevel4 = LCD_DISPCTRL_VBLEV_LEVEL4,
  lcdVBoostLevel5 = LCD_DISPCTRL_VBLEV_LEVEL5,
  lcdVBoostLevel6 = LCD_DISPCTRL_VBLEV_LEVEL6,
  lcdVBoostLevel7 = LCD_DISPCTRL_VBLEV_LEVEL7
}
 
enum  LCD_VLCDSel_TypeDef {
  lcdVLCDSelVDD = LCD_DISPCTRL_VLCDSEL_VDD,
  lcdVLCDSelVExtBoost = LCD_DISPCTRL_VLCDSEL_VEXTBOOST
}
 
enum  LCD_Wave_TypeDef {
  lcdWaveLowPower = LCD_DISPCTRL_WAVE_LOWPOWER,
  lcdWaveNormal = LCD_DISPCTRL_WAVE_NORMAL
}
 

Functions

__STATIC_INLINE void LCD_AnimEnable (bool enable)
 Enables or disables LCD Animation feature.
 
void LCD_AnimInit (const LCD_AnimInit_TypeDef *animInit)
 Configure the LCD controller Animation feature.
 
__STATIC_INLINE int LCD_AnimState (void)
 Returns current animation state.
 
void LCD_BiasComSet (int comLine, int biasLevel)
 Configure the bias level for a specific segment line.
 
void LCD_BiasSegmentSet (int segmentLine, int biasLevel)
 Configure the bias level for a specific segment line for Direct Segment Control.
 
void LCD_BiasSet (LCD_Bias_TypeDef bias)
 Configure the bias level on the LCD panel.
 
__STATIC_INLINE void LCD_BlankEnable (bool enable)
 Disables all segments, while keeping segment state.
 
__STATIC_INLINE void LCD_BlinkEnable (bool enable)
 Enables or disables LCD blink.
 
__STATIC_INLINE int LCD_BlinkState (void)
 Returns current blink state.
 
void LCD_ContrastSet (int level)
 Configure the contrast level on the LCD panel.
 
__STATIC_INLINE void LCD_DSCEnable (bool enable)
 Enable or disable LCD Direct Segment Control.
 
__STATIC_INLINE void LCD_Enable (bool enable)
 Enable or disable LCD controller.
 
__STATIC_INLINE void LCD_FrameCountEnable (bool enable)
 Enables or disables LCD Frame Control.
 
void LCD_FrameCountInit (const LCD_FrameCountInit_TypeDef *fcInit)
 Initialize the LCD Frame Counter.
 
__STATIC_INLINE void LCD_FreezeEnable (bool enable)
 When set, LCD registers will not be updated until cleared.
 
void LCD_Init (const LCD_Init_TypeDef *lcdInit)
 Initialize the Liquid Crystal Display (LCD) controller.
 
__STATIC_INLINE void LCD_IntClear (uint32_t flags)
 Clear one or more interrupt flags.
 
__STATIC_INLINE void LCD_IntDisable (uint32_t flags)
 Disable LCD interrupts.
 
__STATIC_INLINE void LCD_IntEnable (uint32_t flags)
 Enable LCD interrupts.
 
__STATIC_INLINE uint32_t LCD_IntGet (void)
 Get pending LCD interrupt flags.
 
__STATIC_INLINE uint32_t LCD_IntGetEnabled (void)
 Get enabled and pending LCD interrupt flags.
 
__STATIC_INLINE void LCD_IntSet (uint32_t flags)
 Set one or more pending LCD interrupts from SW.
 
void LCD_SegmentRangeEnable (LCD_SegmentRange_TypeDef segmentRange, bool enable)
 Enables updating this range of LCD segment lines.
 
void LCD_SegmentSet (int com, int bit, bool enable)
 Turn on or clear a segment.
 
void LCD_SegmentSetHigh (int com, uint32_t mask, uint32_t bits)
 Update the high (32-39) segments on a given COM-line in one operation.
 
void LCD_SegmentSetLow (int com, uint32_t mask, uint32_t bits)
 Update 0-31 lowest segments on a given COM-line in one operation according to the bit mask.
 
__STATIC_INLINE void LCD_SyncBusyDelay (uint32_t flags)
 Polls LCD SYNCBUSY flags, until flag has been cleared.
 
__STATIC_INLINE uint32_t LCD_SyncBusyGet (void)
 Returns SYNCBUSY bits, indicating which registers have pending updates.
 
void LCD_UpdateCtrl (LCD_UpdateCtrl_TypeDef ud)
 Configure Update Control.
 
void LCD_VBoostSet (LCD_VBoostLevel_TypeDef vboost)
 Configure voltage booster.
 
void LCD_VLCDSelect (LCD_VLCDSel_TypeDef vlcd)
 Select a source for VLCD.
 

Macro Definition Documentation

#define LCD_INIT_DEFAULT
Value:
{ \
true, \
lcdMuxQuadruplex, \
lcdBiasOneThird, \
lcdWaveLowPower, \
lcdVLCDSelVDD, \
lcdConConfVLCD, \
}

Default configuration for LCD initialization structure, enables 160 segments.

Definition at line 297 of file em_lcd.h.

Enumeration Type Documentation

Animation Logic Control, how AReg and BReg should be combined.

Enumerator
lcdAnimLogicAnd 

Use bitwise logic AND to mix animation register A (AREGA) and B (AREGB).

lcdAnimLogicOr 

Use bitwise logic OR to mix animation register A (AREGA) and B (AREGB).

Definition at line 219 of file em_lcd.h.

Animation Shift operation; none, left or right.

Enumerator
lcdAnimShiftNone 

No shift.

lcdAnimShiftLeft 

Shift segment bits left.

lcdAnimShiftRight 

Shift segment bits right.

Definition at line 209 of file em_lcd.h.

Bias setting.

Enumerator
lcdBiasStatic 

Static (2 levels).

lcdBiasOneHalf 

1/2 Bias (3 levels).

lcdBiasOneThird 

1/3 Bias (4 levels).

lcdBiasOneFourth 

1/4 Bias (5 levels).

Definition at line 97 of file em_lcd.h.

Contrast Configuration.

Enumerator
lcdConConfVLCD 

Contrast is adjusted relative to VDD (VLCD).

lcdConConfGND 

Contrast is adjusted relative to Ground.

Definition at line 122 of file em_lcd.h.

Frame Counter Clock Prescaler, FC-CLK = FrameRate (Hz) / this factor.

Enumerator
lcdFCPrescDiv1 

Prescale Div 1.

lcdFCPrescDiv2 

Prescale Div 2.

lcdFCPrescDiv4 

Prescale Div 4.

lcdFCPrescDiv8 

Prescale Div 8.

Definition at line 154 of file em_lcd.h.

MUX setting.

Enumerator
lcdMuxStatic 

Static (segments can be multiplexed with LCD_COM[0]).

lcdMuxDuplex 

Duplex / 1/2 Duty cycle (segments can be multiplexed with LCD_COM[0:1]).

lcdMuxTriplex 

Triplex / 1/3 Duty cycle (segments can be multiplexed with LCD_COM[0:2]).

lcdMuxQuadruplex 

Quadruplex / 1/4 Duty cycle (segments can be multiplexed with LCD_COM[0:3]).

lcdMuxSextaplex 

Sextaplex / 1/6 Duty cycle (segments can be multiplexed with LCD_COM[0:5]).

lcdMuxOctaplex 

Octaplex / 1/6 Duty cycle (segments can be multiplexed with LCD_COM[0:5]).

Definition at line 66 of file em_lcd.h.

Segment selection.

Enumerator
lcdSegment0_3 

Select segment lines 0 to 3.

lcdSegment4_7 

Select segment lines 4 to 7.

lcdSegment8_11 

Select segment lines 8 to 11.

lcdSegment12_15 

Select segment lines 12 to 15.

lcdSegment16_19 

Select segment lines 16 to 19.

lcdSegment20_23 

Select segment lines 20 to 23.

lcdSegment24_27 

Select segment lines 24 to 27.

lcdSegment28_31 

Select segment lines 28 to 31.

lcdSegment32_35 

Select segment lines 32 to 35.

lcdSegment36_39 

Select segment lines 36 to 39.

lcdSegmentAll 

Select all segment lines.

Definition at line 167 of file em_lcd.h.

Update Data Control.

Enumerator
lcdUpdateCtrlRegular 

Regular update, data transfer done immediately.

lcdUpdateCtrlFCEvent 

Data transfer done at Frame Counter event.

lcdUpdateCtrlFrameStart 

Data transfer done at Frame Start.

Definition at line 199 of file em_lcd.h.

Voltage Boost Level - Data sheets document setting for each part number.

Enumerator
lcdVBoostLevel0 

Voltage boost LEVEL0.

lcdVBoostLevel1 

Voltage boost LEVEL1.

lcdVBoostLevel2 

Voltage boost LEVEL2.

lcdVBoostLevel3 

Voltage boost LEVEL3.

lcdVBoostLevel4 

Voltage boost LEVEL4.

lcdVBoostLevel5 

Voltage boost LEVEL5.

lcdVBoostLevel6 

Voltage boost LEVEL6.

lcdVBoostLevel7 

Voltage boost LEVEL7.

Definition at line 132 of file em_lcd.h.

VLCD Voltage Source.

Enumerator
lcdVLCDSelVDD 

VLCD Powered by VDD.

lcdVLCDSelVExtBoost 

VLCD Powered by external VDD / Voltage Boost.

Definition at line 112 of file em_lcd.h.

Wave type.

Enumerator
lcdWaveLowPower 

Low power optimized waveform output.

lcdWaveNormal 

Regular waveform output

Definition at line 89 of file em_lcd.h.

Function Documentation

__STATIC_INLINE void LCD_AnimEnable ( bool  enable)

Enables or disables LCD Animation feature.

Parameters
[in]enableBoolean true enables animation, false disables animation.

Definition at line 381 of file em_lcd.h.

Referenced by LCD_AnimInit().

void LCD_AnimInit ( const LCD_AnimInit_TypeDef animInit)

Configure the LCD controller Animation feature.

Parameters
[in]animInitA pointer to the LCD Animation initialization structure.

Definition at line 199 of file em_lcd.c.

References LCD_AnimInit_TypeDef::animLogic, LCD_AnimInit_TypeDef::AReg, LCD_AnimInit_TypeDef::AShift, LCD_AnimInit_TypeDef::BReg, LCD_AnimInit_TypeDef::BShift, LCD_AnimInit_TypeDef::enable, LCD_AnimEnable(), and LCD_AnimInit_TypeDef::startSeg.

__STATIC_INLINE int LCD_AnimState ( void  )

Returns current animation state.

Returns
Animation state, in range 0-15.

Definition at line 445 of file em_lcd.h.

void LCD_BiasComSet ( int  comLine,
int  biasLevel 
)

Configure the bias level for a specific segment line.

Note
When DSC is active, each configuration takes up 4 bits in the Segment Registers (SEGD4L/SEGD4H) which defines bias level. For optimal use of this feature, the entire SEGD-registers should be set at once in a optimized routine. Therefore, this function shows how to correctly configure the bias levels and should be used with care.
Parameters
[in]comLineA COM line number, 0-7.
[in]biasLevelThe bias configuration level, 0-4. This value must be within the constraints defined by the LCD_DISPCTRL bias settings. For more information, see the appropriate Reference Manual and data sheet.

Definition at line 762 of file em_lcd.c.

void LCD_BiasSegmentSet ( int  segmentLine,
int  biasLevel 
)

Configure the bias level for a specific segment line for Direct Segment Control.

Note
When DSC is active, each configuration takes up 4 bits in the Segment Registers (SEGD0L/SEGD1H) which defines the bias level. For optimal use of this feature, the entire SEGD-registers should be set at once in an optimized routine. Therefore, this function shows how to correctly configure the bias levels and should be used with care.
Parameters
[in]segmentLineA segment line number.
[in]biasLevelThe bias configuration level, 0-4. This value must be within the constraints defined by the LCD_DISPCTRL bias settings. For more information, see the applicable Reference Manual and data sheet.

Definition at line 658 of file em_lcd.c.

void LCD_BiasSet ( LCD_Bias_TypeDef  bias)

Configure the bias level on the LCD panel.

Parameters
[in]biasThe bias level.

Definition at line 615 of file em_lcd.c.

__STATIC_INLINE void LCD_BlankEnable ( bool  enable)

Disables all segments, while keeping segment state.

Parameters
[in]enableBoolean true clears all segments, boolean false restores all segment lines.

Definition at line 413 of file em_lcd.h.

__STATIC_INLINE void LCD_BlinkEnable ( bool  enable)

Enables or disables LCD blink.

Parameters
[in]enableBoolean true enables blink, false disables blink.

Definition at line 397 of file em_lcd.h.

__STATIC_INLINE int LCD_BlinkState ( void  )

Returns current blink state.

Returns
Return value is 1 if segments are enabled, 0 if disabled.

Definition at line 457 of file em_lcd.h.

void LCD_ContrastSet ( int  level)

Configure the contrast level on the LCD panel.

Parameters
[in]levelThe contrast level in range 0-31.

Definition at line 582 of file em_lcd.c.

Referenced by LCD_Init().

__STATIC_INLINE void LCD_DSCEnable ( bool  enable)

Enable or disable LCD Direct Segment Control.

Parameters
[in]enableIf true, enables LCD controller Direct Segment Control Segment and COM line bias levels need to be set explicitly with LCD_BiasSegmentSet() and LCD_BiasComSet() function calls respectively.

Definition at line 613 of file em_lcd.h.

__STATIC_INLINE void LCD_Enable ( bool  enable)

Enable or disable LCD controller.

Parameters
[in]enableIf true, enables LCD controller with current configuration. If false, disables LCD controller. Enable CMU clock for LCD for correct operation.

Definition at line 365 of file em_lcd.h.

Referenced by LCD_Init(), and SegmentLCD_Disable().

__STATIC_INLINE void LCD_FrameCountEnable ( bool  enable)

Enables or disables LCD Frame Control.

Parameters
[in]enableBoolean true enables frame counter, false disables frame counter.

Definition at line 429 of file em_lcd.h.

Referenced by LCD_FrameCountInit().

void LCD_FrameCountInit ( const LCD_FrameCountInit_TypeDef fcInit)

Initialize the LCD Frame Counter.

Parameters
[in]fcInitA pointer to the Frame Counter initialization structure.

Definition at line 171 of file em_lcd.c.

References LCD_FrameCountInit_TypeDef::enable, LCD_FrameCountEnable(), LCD_FrameCountInit_TypeDef::prescale, and LCD_FrameCountInit_TypeDef::top.

__STATIC_INLINE void LCD_FreezeEnable ( bool  enable)

When set, LCD registers will not be updated until cleared.

Parameters
[in]enableWhen enable is true, update is stopped; when false, all registers are updated.

Definition at line 470 of file em_lcd.h.

Referenced by SegmentLCD_Number(), SegmentLCD_UnsignedHex(), and SegmentLCD_Write().

void LCD_Init ( const LCD_Init_TypeDef lcdInit)

Initialize the Liquid Crystal Display (LCD) controller.

Configures the LCD controller. You must enable it afterwards, potentially configuring Frame Control and interrupts first according to requirements.

Parameters
[in]lcdInitA pointer to the initialization structure which configures the LCD controller.

Definition at line 65 of file em_lcd.c.

References LCD_Init_TypeDef::bias, LCD_Init_TypeDef::contrast, LCD_Init_TypeDef::enable, LCD_ContrastSet(), LCD_Enable(), LCD_Init_TypeDef::mux, LCD_Init_TypeDef::vlcd, and LCD_Init_TypeDef::wave.

Referenced by SegmentLCD_Init().

__STATIC_INLINE void LCD_IntClear ( uint32_t  flags)

Clear one or more interrupt flags.

Parameters
[in]flagsLCD interrupt sources to clear. Use a set of interrupt flags OR-ed together to clear multiple interrupt sources for LCD module (LCD_IFS_nnn).

Definition at line 598 of file em_lcd.h.

__STATIC_INLINE void LCD_IntDisable ( uint32_t  flags)

Disable LCD interrupts.

Parameters
[in]flagsLCD interrupt sources to disable. Use a set of interrupt flags OR-ed together to disable multiple interrupt sources for LCD module (LCD_IFS_nnn).

Definition at line 584 of file em_lcd.h.

Referenced by SegmentLCD_Init().

__STATIC_INLINE void LCD_IntEnable ( uint32_t  flags)

Enable LCD interrupts.

Parameters
[in]flagsLCD interrupt sources to enable. Use a set of interrupt flags OR-ed together to set multiple interrupt sources for LCD module (LCD_IFS_nnn).

Definition at line 570 of file em_lcd.h.

__STATIC_INLINE uint32_t LCD_IntGet ( void  )

Get pending LCD interrupt flags.

Returns
Pending LCD interrupt sources. Returns a set of interrupt flags OR-ed together for multiple interrupt sources in the LCD module (LCD_IFS_nnn).

Definition at line 512 of file em_lcd.h.

__STATIC_INLINE uint32_t LCD_IntGetEnabled ( void  )

Get enabled and pending LCD interrupt flags.

Useful for handling more interrupt sources in the same interrupt handler.

Note
Event bits are not cleared by the use of this function.
Returns
Pending and enabled LCD interrupt sources. Return value is the bitwise AND combination of
  • the OR combination of enabled interrupt sources in LCD_IEN_nnn register (LCD_IEN_nnn) and
  • the bitwise OR combination of valid interrupt flags of LCD module (LCD_IF_nnn).

Definition at line 535 of file em_lcd.h.

__STATIC_INLINE void LCD_IntSet ( uint32_t  flags)

Set one or more pending LCD interrupts from SW.

Parameters
[in]flagsLCD interrupt sources to set to pending. Use a set of interrupt flags OR-ed together to set multiple interrupt sources for the LCD module (LCD_IFS_nnn).

Definition at line 556 of file em_lcd.h.

void LCD_SegmentRangeEnable ( LCD_SegmentRange_TypeDef  segmentRange,
bool  enable 
)

Enables updating this range of LCD segment lines.

Parameters
[in]segmentRangeA range of 4 LCD segment lines to enable or disable for all enabled COM lines.
[in]enableBoolean true to enable segment updates, false to disable updates.

Definition at line 247 of file em_lcd.c.

void LCD_SegmentSet ( int  com,
int  bit,
bool  enable 
)

Turn on or clear a segment.

Note
For the Gecko Family, the maximum configuration is (COM-lines x Segment-Lines) 4x40. For the Tiny Gecko Family, the maximum configuration is 8x20 or 4x24. For the Giant Gecko Family, the maximum configuration is 8x36 or 4x40.
Parameters
[in]comA COM line to change.
[in]bitA bit index indicating which field to change.
[in]enableTrue will set segment, false will clear segment.

Definition at line 275 of file em_lcd.c.

References BUS_RegBitWrite().

Referenced by displayBlock(), SegmentLCD_ARing(), SegmentLCD_Battery(), SegmentLCD_EnergyMode(), SegmentLCD_Number(), SegmentLCD_Symbol(), SegmentLCD_UnsignedHex(), and SegmentLCD_Write().

void LCD_SegmentSetHigh ( int  com,
uint32_t  mask,
uint32_t  bits 
)

Update the high (32-39) segments on a given COM-line in one operation.

Parameters
[in]comIndicates a COM line to update.
[in]maskA bit mask for segments 32-39.
[in]bitsA bit pattern for segments 32-39.

Definition at line 500 of file em_lcd.c.

void LCD_SegmentSetLow ( int  com,
uint32_t  mask,
uint32_t  bits 
)

Update 0-31 lowest segments on a given COM-line in one operation according to the bit mask.

Parameters
[in]comIndicates a COM line to update.
[in]maskA bit mask for segments 0-31.
[in]bitsA bit pattern for segments 0-31.

Definition at line 411 of file em_lcd.c.

__STATIC_INLINE void LCD_SyncBusyDelay ( uint32_t  flags)

Polls LCD SYNCBUSY flags, until flag has been cleared.

Parameters
[in]flagsBit fields for LCD registers that will be updated before we continue.

Definition at line 498 of file em_lcd.h.

Referenced by SegmentLCD_Disable(), SegmentLCD_Init(), SegmentLCD_Number(), SegmentLCD_UnsignedHex(), and SegmentLCD_Write().

__STATIC_INLINE uint32_t LCD_SyncBusyGet ( void  )

Returns SYNCBUSY bits, indicating which registers have pending updates.

Returns
Bit fields for LCD registers that have pending updates.

Definition at line 486 of file em_lcd.h.

void LCD_UpdateCtrl ( LCD_UpdateCtrl_TypeDef  ud)

Configure Update Control.

Parameters
[in]udConfigures the LCD update method.

Definition at line 159 of file em_lcd.c.

void LCD_VBoostSet ( LCD_VBoostLevel_TypeDef  vboost)

Configure voltage booster.

The resulting voltage level is described in each part number's data sheet

Parameters
[in]vboostVoltage boost level

Definition at line 630 of file em_lcd.c.

Referenced by SegmentLCD_Init().

void LCD_VLCDSelect ( LCD_VLCDSel_TypeDef  vlcd)

Select a source for VLCD.

Parameters
[in]vlcdSelect a source for the VLCD voltage.

Definition at line 131 of file em_lcd.c.

References lcdVLCDSelVDD, and lcdVLCDSelVExtBoost.

Referenced by SegmentLCD_Init().