HFXO initialization structure. Initialization values should be obtained from a configuration tool, app note, or xtal data sheet.
Definition at line 2413
of file em_cmu.h
.
#include <
em_cmu.h
>
Data Fields | |
uint8_t | boost |
bool | glitchDetector |
CMU_OscMode_TypeDef | mode |
uint8_t | timeout |
Field Documentation
uint8_t CMU_HFXOInit_TypeDef::boost |
HFXO Boost, 0=50% 1=70%, 2=80%, 3=100%
Definition at line 2438
of file em_cmu.h
.
Referenced by CMU_HFXOInit().
bool CMU_HFXOInit_TypeDef::glitchDetector |
Enable/disable glitch detector
Definition at line 2440
of file em_cmu.h
.
Referenced by CMU_HFXOInit().
CMU_OscMode_TypeDef CMU_HFXOInit_TypeDef::mode |
uint8_t CMU_HFXOInit_TypeDef::timeout |
The documentation for this struct was generated from the following file:
- C:/HandsOn/super/platform/emlib/inc/
em_cmu.h