BCP_PacketHeader Struct Reference
BCP Packet Header definition.
Definition at line 114
of file bsp_bcp.h
.
#include <
bsp_bcp.h
>
Data Fields | |
uint8_t | magic |
uint8_t | payloadLength |
uint8_t | reserved |
uint8_t | type |
Field Documentation
uint8_t BCP_PacketHeader::magic |
Magic - start of packet - must be BSP_BCP_MAGIC
Definition at line 115
of file bsp_bcp.h
.
uint8_t BCP_PacketHeader::payloadLength |
Length of data segment >=0 and <=BSP_BCP_PACKET_SIZE
Definition at line 117
of file bsp_bcp.h
.
uint8_t BCP_PacketHeader::reserved |
Reserved for future expansion
Definition at line 118
of file bsp_bcp.h
.
uint8_t BCP_PacketHeader::type |
Type - packet type
Definition at line 116
of file bsp_bcp.h
.
The documentation for this struct was generated from the following file:
- C:/HandsOn/super/hardware/kit/common/bsp/
bsp_bcp.h