ADC initialization structure, common for single conversion and scan sequence.
Definition at line 782
of file em_adc.h
.
#include <
em_adc.h
>
Data Fields | |
ADC_LPFilter_TypeDef | lpfMode |
ADC_OvsRateSel_TypeDef | ovsRateSel |
uint8_t | prescale |
bool | tailgate |
uint8_t | timebase |
ADC_Warmup_TypeDef | warmUpMode |
Field Documentation
ADC_LPFilter_TypeDef ADC_Init_TypeDef::lpfMode |
Lowpass or decoupling capacitor filter.
Definition at line 791
of file em_adc.h
.
Referenced by ADC_Init().
ADC_OvsRateSel_TypeDef ADC_Init_TypeDef::ovsRateSel |
Oversampling rate select. To have any effect, oversampling must be enabled for single/scan mode.
Definition at line 787
of file em_adc.h
.
Referenced by ADC_Init(), and TOUCH_Init().
uint8_t ADC_Init_TypeDef::prescale |
Clock division factor N, ADC clock = (HFPERCLK or HFPERCCLK) / (N + 1).
Definition at line 807
of file em_adc.h
.
Referenced by ADC_Init(), adcInit(), MIC_init(), and TOUCH_Init().
bool ADC_Init_TypeDef::tailgate |
Enable/disable conversion tailgating.
Definition at line 810
of file em_adc.h
.
Referenced by ADC_Init().
uint8_t ADC_Init_TypeDef::timebase |
Timebase for ADC warm up. Select N to give (N+1) HFPERCLK / HFPERCCLK cycles. (Additional delay is added for bandgap references. See the reference manual for more information.) Normally, N should be selected so that the timebase is at least 1 us. See ADC_TimebaseCalc() to obtain a suggested timebase of, at least, 1 us.
Definition at line 804
of file em_adc.h
.
Referenced by ADC_Init(), adcInit(), and MIC_init().
ADC_Warmup_TypeDef ADC_Init_TypeDef::warmUpMode |
The documentation for this struct was generated from the following file:
- C:/HandsOn/super/platform/emlib/inc/
em_adc.h