Detailed Description

Utility functions.

Macros

#define UTIL_SUPPLY_TYPE_AA 2
#define UTIL_SUPPLY_TYPE_AAA 3
#define UTIL_SUPPLY_TYPE_CR2032 4
#define UTIL_SUPPLY_TYPE_UNKNOWN 0
#define UTIL_SUPPLY_TYPE_USB 1

Functions

static void adcDeInit (void)
De-initializes the A/D converter.
static void adcInit (void)
Initializes the A/D converter.
static uint16_t getAdcSample (void)
Initiates an A/D conversion and reads the sample when done.
static float measureSupplyIR (uint8_t loadSetting)
Measures the unladed and loaded supply voltage and calculates the intermal resistance of the connected supply. The load is provided by the heater element built in the Si7021.
static float measureSupplyVoltage (unsigned int avg)
Measures the supply voltage by averaging multiple readings.
void SysTick_Handler (void)
Interrupt Service Routine for system tick counter.
static void timer_callback ( sl_sleeptimer_timer_handle_t *handle, void *data)
sleeptmer callback function, called when the timer expired.
void UTIL_delay (uint32_t ms)
Delays number of msTick Systicks (1 ms)
uint32_t UTIL_init (void)
Sets up the SysTick timer for 1ms interrupts and initializes and starts the RTC timer.
bool UTIL_isLowPower (void)
Checks if the current power supply has low power capability.
void UTIL_shutdown (void)
Enter lowest power shutdown mode, EM4S.
void UTIL_sleep (uint32_t ms)
Delays number of milliseconds in sleep mode (EM2) using the sleeptimer.
uint32_t UTIL_sleepInit (void)
Sets up the sleeptimer used for sleep functions.
void UTIL_supplyGetCharacteristics (uint8_t *type, float *voltage, float *ir)
Retrieves the supply characteristic variables.
uint8_t UTIL_supplyGetType (void)
Returns the type of the power supply.
void UTIL_supplyProbe (void)
Probes the connected supply and determines its type. The results are stored in global variables.
uint32_t UTIL_waitForEvent (uint32_t ms)
Delays number of milliseconds in sleep mode (EM2) using the sleeptimer but returns if an event wakes up the MCU.

Macro Definition Documentation

#define UTIL_SUPPLY_TYPE_AA   2

The board powered from AA batteries

Definition at line 49 of file util.h .

#define UTIL_SUPPLY_TYPE_AAA   3

The board powered from AAA batteries

Definition at line 50 of file util.h .

Referenced by UTIL_supplyProbe() .

#define UTIL_SUPPLY_TYPE_CR2032   4

The board powered from a CR2032 battery

Definition at line 51 of file util.h .

Referenced by UTIL_isLowPower() , and UTIL_supplyProbe() .

#define UTIL_SUPPLY_TYPE_UNKNOWN   0

Unknown power supply type

Definition at line 47 of file util.h .

Referenced by UTIL_isLowPower() , and UTIL_supplyProbe() .

#define UTIL_SUPPLY_TYPE_USB   1

The board powered from the USB connector

Definition at line 48 of file util.h .

Referenced by UTIL_supplyProbe() .

Function Documentation

static void adcDeInit ( void )
static

De-initializes the A/D converter.

Returns
None

Definition at line 106 of file util_supply.c .

References PRS_SourceAsyncSignalSet() .

Referenced by measureSupplyVoltage() .

static uint16_t getAdcSample ( void )
static

Initiates an A/D conversion and reads the sample when done.

Returns
The output of the A/D conversion

Definition at line 121 of file util_supply.c .

References ADC_DataSingleGet() , ADC_IntGet() , ADC_Start() , and adcStartSingle .

Referenced by measureSupplyVoltage() .

static float measureSupplyIR ( uint8_t loadSetting )
static

Measures the unladed and loaded supply voltage and calculates the intermal resistance of the connected supply. The load is provided by the heater element built in the Si7021.

Parameters
[in] loadSetting Heater current setting of the Si7021
Returns
The measured internal resistance of the connected supply

Definition at line 174 of file util_supply.c .

References measureSupplyVoltage() , SI7021_CMD_WRITE_HEATER_CTRL , SI7021_CMD_WRITE_USER_REG1 , SI7021_cmdWrite() , and UTIL_delay() .

Referenced by UTIL_supplyProbe() .

static float measureSupplyVoltage ( unsigned int avg )
static

Measures the supply voltage by averaging multiple readings.

Parameters
[in] avg Number of measurements to average
Returns
The measured voltage

Definition at line 140 of file util_supply.c .

References adcDeInit() , adcInit() , and getAdcSample() .

Referenced by measureSupplyIR() , and UTIL_supplyProbe() .

void SysTick_Handler ( void )

Interrupt Service Routine for system tick counter.

Returns
None

Definition at line 82 of file util.c .

uint32_t UTIL_init ( void )

Sets up the SysTick timer for 1ms interrupts and initializes and starts the RTC timer.

Returns
Returns zero on OK, non-zero otherwise

Definition at line 63 of file util.c .

References CMU_ClockFreqGet() , and cmuClock_CORE .

bool UTIL_isLowPower ( void )

Checks if the current power supply has low power capability.

Returns
True if the supply is low power type, false otherwise

Definition at line 294 of file util_supply.c .

References UTIL_SUPPLY_TYPE_CR2032 , and UTIL_SUPPLY_TYPE_UNKNOWN .

void UTIL_shutdown ( void )

Enter lowest power shutdown mode, EM4S.

Returns
None

Definition at line 118 of file util.c .

References EMU_EM4Init() , EMU_EM4INIT_DEFAULT , EMU_EnterEM4() , GPIO_EM4EnablePinWakeup() , GPIO_PinModeSet() , and gpioModeInputPullFilter .

void UTIL_sleep ( uint32_t ms )

Delays number of milliseconds in sleep mode (EM2) using the sleeptimer.

Parameters
ms Number of milliseconds to sleep.
Returns
None

Definition at line 91 of file util_sleep.c .

References EMU_EnterEM2() , sl_sleeptimer_start_timer_ms() , and timer_callback() .

uint32_t UTIL_sleepInit ( void )

Sets up the sleeptimer used for sleep functions.

Returns
Returns zero on OK, non-zero otherwise.

Definition at line 74 of file util_sleep.c .

References sl_sleeptimer_init() .

void UTIL_supplyGetCharacteristics ( uint8_t * type,
float * voltage,
float * ir
)

Retrieves the supply characteristic variables.

Parameters
[in] type Supply type
[in] voltage Loaded supply voltage
[in] ir Internal resistance of the supply
Returns
None

Definition at line 266 of file util_supply.c .

uint8_t UTIL_supplyGetType ( void )

Returns the type of the power supply.

Returns
The type of the supply

Definition at line 282 of file util_supply.c .

void UTIL_supplyProbe ( void )

Probes the connected supply and determines its type. The results are stored in global variables.

Returns
None

Definition at line 221 of file util_supply.c .

References measureSupplyIR() , measureSupplyVoltage() , SI7021_deInit() , SI7021_init() , UTIL_SUPPLY_TYPE_AAA , UTIL_SUPPLY_TYPE_CR2032 , UTIL_SUPPLY_TYPE_UNKNOWN , and UTIL_SUPPLY_TYPE_USB .

uint32_t UTIL_waitForEvent ( uint32_t ms )

Delays number of milliseconds in sleep mode (EM2) using the sleeptimer but returns if an event wakes up the MCU.

Parameters
ms The maximum number of milliseconds to sleep.
Returns
The number of milliseconds remained from the wait.

Definition at line 112 of file util_sleep.c .

References EMU_EnterEM2() , sl_sleeptimer_get_timer_time_remaining() , sl_sleeptimer_start_timer_ms() , sl_sleeptimer_stop_timer() , sl_sleeptimer_tick_to_ms() , and timer_callback() .