LESENSE peripheral control descriptor structure.
Definition at line 565
of file em_lesense.h
.
#include <
em_lesense.h
>
Field Documentation
LESENSE_ControlACMP_TypeDef LESENSE_PerCtrlDesc_TypeDef::acmp0Mode |
Configure how LESENSE controls ACMP 0.
Definition at line 605
of file em_lesense.h
.
Referenced by LESENSE_Init().
LESENSE_ControlACMP_TypeDef LESENSE_PerCtrlDesc_TypeDef::acmp1Mode |
Configure how LESENSE controls ACMP 1.
Definition at line 608
of file em_lesense.h
.
Referenced by LESENSE_Init().
LESENSE_ControlDACConv_TypeDef LESENSE_PerCtrlDesc_TypeDef::dacCh0ConvMode |
Configure how LESENSE controls conversion on DAC channel 0.
Definition at line 571
of file em_lesense.h
.
Referenced by LESENSE_Init().
LESENSE_ControlDACData_TypeDef LESENSE_PerCtrlDesc_TypeDef::dacCh0Data |
Configure DAC channel 0 data control.
Definition at line 567
of file em_lesense.h
.
Referenced by LESENSE_Init().
LESENSE_ControlDACOut_TypeDef LESENSE_PerCtrlDesc_TypeDef::dacCh0OutMode |
Configure how LESENSE controls output on DAC channel 0.
Definition at line 576
of file em_lesense.h
.
Referenced by LESENSE_Init().
LESENSE_ControlDACConv_TypeDef LESENSE_PerCtrlDesc_TypeDef::dacCh1ConvMode |
Configure how LESENSE controls conversion on DAC channel 1.
Definition at line 584
of file em_lesense.h
.
Referenced by LESENSE_Init().
LESENSE_ControlDACData_TypeDef LESENSE_PerCtrlDesc_TypeDef::dacCh1Data |
Configure DAC channel 1 data control.
Definition at line 580
of file em_lesense.h
.
Referenced by LESENSE_Init().
LESENSE_ControlDACOut_TypeDef LESENSE_PerCtrlDesc_TypeDef::dacCh1OutMode |
Configure how LESENSE controls output on DAC channel 1.
Definition at line 589
of file em_lesense.h
.
Referenced by LESENSE_Init().
uint8_t LESENSE_PerCtrlDesc_TypeDef::dacPresc |
Configure the prescaling factor for the LESENSE - DAC interface. Valid range: 0-31 (5-bit).
Definition at line 595
of file em_lesense.h
.
Referenced by LESENSE_Init().
LESENSE_DACRef_TypeDef LESENSE_PerCtrlDesc_TypeDef::dacRef |
Configure the DAC reference to be used. Set to lesenseDACRefVdd to use VDD and set to lesenseDACRefBandGap to use band gap as reference.
Definition at line 601
of file em_lesense.h
.
Referenced by LESENSE_Init().
LESENSE_WarmupMode_TypeDef LESENSE_PerCtrlDesc_TypeDef::warmupMode |
Configure how LESENSE controls ACMPs and DAC in idle mode.
Definition at line 611
of file em_lesense.h
.
Referenced by LESENSE_Init().
The documentation for this struct was generated from the following file:
- C:/HandsOn/super/platform/emlib/inc/
em_lesense.h