BATTERY_TypeDef Struct Reference

Defines segment COM and BIT fields for Battery (suited for Anim)

Definition at line 128 of file segmentlcd.c.

Data Fields

uint8_t bit [4]
 
uint8_t com [4]
 

Field Documentation

uint8_t BATTERY_TypeDef::bit[4]

LCD bit number

Definition at line 130 of file segmentlcd.c.

Referenced by SegmentLCD_Battery().

uint8_t BATTERY_TypeDef::com[4]

LCD COM line (for multiplexing)

Definition at line 129 of file segmentlcd.c.

Referenced by SegmentLCD_Battery().


The documentation for this struct was generated from the following file:
  • C:/HandsOn/super/hardware/kit/common/drivers/segmentlcd.c