EUSART_IrDAInit_TypeDef Struct Reference

IrDA Initialization structure.

Definition at line 259 of file em_eusart.h .

#include < em_eusart.h >

Data Fields

EUSART_UartInit_TypeDef init
General EUSART initialization structure.
bool irDALowFrequencyEnable
Enable the IrDA low frequency mode. Only Rx operation are enabled.
EUSART_IrDAPulseWidth_Typedef irDAPulseWidth
EUSART_IrDARxFilterEnable_TypeDef irDARxFilterEnable
Set to enable filter on IrDA demodulator.

Field Documentation

EUSART_IrDAPulseWidth_Typedef EUSART_IrDAInit_TypeDef::irDAPulseWidth

Configure the pulse width generated by the IrDA modulator as a fraction of the configured EUSART bit period.

Definition at line 271 of file em_eusart.h .


The documentation for this struct was generated from the following file:
  • C:/repos/super/platform/emlib/inc/ em_eusart.h