Wi-Fi Commissioning Demonstration
For the demo purposes, the WF200/WFM200 concurrently exposes 2 Wi-Fi interfaces:
- A SoftAP (Software Enabled Access Point) interface to accept incoming connections from Wi-Fi Devices
- A Station interface to connect to Wi-Fi APs (Access Points)
The host supports a Web server which exposes a user-accessible Web page. 'Commissioning' means providing the AP 's credentials to the Station over a temporary SoftAP connection from a Wi-Fi Device . This is achieved via the Web page.
At this moment:
- Your Device is not connected to the SoftAP (it may be connected to another AP )
- The SoftAP is waiting for a Device to connect
- The Station is not connected to any AP
Connecting to the SoftAP
When the SoftAP is started, you can join it with any Wi-Fi Device :
- On your Device , scan for Wi-Fi networks
- Select the silabs-pi-demo network
- Password: CHANGE_ME
- In a navigator, browse to http://192.168.5.1
From this Web page you can read and toggle the state of the onboard LEDs.
At this moment:
- Your Device is connected to the SoftAP
- The Station is not connected to any AP
Commissioning Web Page
The page allows:
- Control of the Raspberry Pi LEDs (used to confirm that you are connected to your kit)
-
Control of the WF(M)200
Station
:
- Scan for nearby networks' AP s
- Connect to a selected AP
- Disconnect from the AP
Scanning for Nearby Networks
In the 'Wi-Fi Access Point/Station' panel:
-
Press
Refresh Wi-Fi Scan Resultsto scan for surrounding APs- Existing Wi-Fi networks are listed at the bottom of the panel, with their SSID and reception level
At this moment:
- Your Device is connected to the SoftAP
- The Station is not connected to any AP yet
Connecting the Station to a Home/Office AP
- Select one Wi-Fi network AP
- Enter credentials (if required)
-
Press
Connect -
A popup window appears, indicating connection to the
AP
. Press
OKto close it
The Station status says 'STA Connected' with:
- The Wi-Fi AP 's SSID
- The Station 's IP address on the Home Wi-Fi AP (once it's allocated)
Note: Store this IP address for the next steps.
The kit has been commissioned successfully .
At this moment:
- The Station is connected to the AP
- Your Device is still connected to the SoftAP
If you want to connect the Station to another AP , press 'Disconnect' first.
Indirect Communication with the Kit
- Connect your Device to the same AP you've connected the kit to
- Use the IP address you stored above to connect to the kit and access the Web page again
At this moment
- The Station is connected to the AP
- Your Device is not connected to the SoftAP anymore
- Your Device is indirectly connected to the kit via the AP