WF(M)200 Wi-Fi Expansion Board and EFM32GG11 (STK3701A) Starter Kit
The WF(M)200 Wi-Fi Expansion Kit is the best and fastest way to explore the capabilities of the WF200 Series of Wi-Fi Transceivers. The kit contains an expansion board adding a Wi-Fi connectivity to the STK3701A Starter Kit by plugging them together. This expansion board, composed of a WF(M)200 Wi-Fi Module, allows the connection to a Wi-Fi Network but also provides an Access Point to which other devices can connect.
Examples running on the STK3701A Starter Kit with a WF(M)200 Wi-Fi Expansion Board are listed below: