WF(M)200 Wi-Fi Expansion Board and EFR32MG12 (WSTK6000B) Starter Kit #
The WF(M)200 Wi-Fi Expansion Kit is the best and fastest way to explore the capabilities of the WF200 Series of Wi-Fi Transceivers. The kit contains an expansion board adding a Wi-Fi connectivity to the WSTK6000B Starter Kit by plugging them together. This expansion board, composed of a WF(M)200 Wi-Fi Module, allows the connection to a Wi-Fi Network but also provides an Access Point to which other devices can connect.
Examples running on the WSTK6000B Starter Kit with a WF(M)200 Wi-Fi Expansion Board are listed below: