WGM160P Wi-Fi Module Starter Kit (SLWSTK6121A)
The WGM160P Wi-Fi Module Starter Kit is the best and fastest way to explore the capabilities of the WGM160P Wi-Fi Module, composed of an EFM32GG11 and a WF200. The kit contains a radio module board and a Silicon Labs Wireless STK baseboard (WSTK). The radio module board, composed of a WF200 Wi-Fi Module, allows the connection to a Wi-Fi Network but also provides an Access Point to which other devices can connect.
Examples running on WGM160P Wi-Fi Module Starter Kit are listed below: