Further Steps
Wi-Fi Commissioning Logs
The example outputs logs on the serial port, this logs allows to keep track of the program execution by tracing information about:
- Changes of the Wi-Fi connection status (SoftAP start/stop, Station connection/disconnection, IP address, ...)
- User interactions with the Webpage (LED toggling, Wi-Fi scan, ...)
- Execution errors
The image below illustrates logs displayed in the serial console during a Wi-Fi commissioning process.
Change the Default Settings
By Using the Prompt
By default the application starts by setting up a SoftAP which has hardcoded name. If you want to change the application behavior and directly start as a Station or if you want to start a SoftAP with a different name, a first solution is to press Enter within the 5 seconds after the microcontroller boot to start the prompt. The prompt allows to start in the desired mode and to select the Wi-Fi information (SSID, Passkey and Security mode). Note that this solution is not persistent to reboots or resets.
By Editing and Recompiling the Project
Compared to the previous method, this method is persistent to reboots or resets. The default settings, especially the settings related to the SoftAP (SSID, Passkey, Security mode and IP address) are defined in the lwip_micriumos.h file. You can change the default settings by editing this file, making the needed changes and recompiling the project.
Change the Wi-Fi Communication Bus
From the GitHub Example
The project file of the GitHub example provides 2 configurations to select the Wi-Fi Communication bus (SPI / SDIO) and the compiled binaries related to these configurations are also provided in the binaries folder. Either directly flash the binary corresponding to the desired configuration or select the desired configuration in Simplicity Studio, build the project and flash the device with the generated binary.
Don't forget to put the bus switch of the WF(M)200 Expansion Board accordingly.
From the SDK Example
A difference with the GitHub example is that the SDK example only provides a Debug and a Release configurations and in these configurations the SPI bus is used by default. Nevertheless, it is possible to use the SDIO bus instead by following this procedure:
- Open the Project Properties by selecting the example in the Project Explorer window inside Simplicity Studio 4 and clicking on Project->Properties.
- Open the Symbols tab by clicking on C/C++ General->Paths and Symbols.
- Select GNU C as Language.
- Add the symbol SL_WFX_USE_SDIO with a value of 1.
- Click on Apply and Ok.
- Build the project and flash the device.
Don't forget to put the bus switch of the WF(M)200 Expansion Board accordingly.
Enable the Low Power Feature
From the GitHub Example
Similarly to the bus selection, the project file of the GitHub example provides a configuration enabling the low power on both the MCU and the WF(M)200 chip. Either directly flash the provided binary or select the configuration in Simplicity Studio 4, build the project and flash the device with the generated binary.
You can refer to the AN1219: Power Consumption Measurement Setup and Results on WF(M)200 document to perform measurements on the WF(M)200 chip. Simplicity Studio 4 also provides the Energy Profiler tool, this tool allows to measure the current consumption of a Silicon Labs Starter Kit. The measures being made by the Starter Kit hardware, keep in mind that it is less accurate than a dedicated instrument, nevertheless it provides an idea of the current consumption quickly and easily. For more information about the Energy Profiler, please refer to UG343: Multi-Node Energy Profiler User’s Guide.
Notes:
- This feature is only enabled when the WF(M)200 chip behaves as a Station and is connected to an Access Point while the SoftAP interface is OFF. It is automatically disabled when the SoftAP interface is (re)started.
- Although the MCU low power and the WF(M)200 chip Power Save feature independent from each other, we associated them to ease the example implementation.
- The SDIO bus cannot be used, as is, with the low power feature since the SDIO Out Of Band interrupt pin (GPIO_WIRQ) is not routed to the expander connector.
From the SDK Example
The Low Power feature is not available in the SDK example.
Modify the Webpage
From the GitHub Example
The Webpage sources are provided with the GitHub example in the src/lwip_host/webpage/fs folder when the project imported in Simplicity Studio 4. Notice that it is a symbolic link, the real location on your computer in the cloned repository is Examples/SiliconLabs/commissioning/webpage.
Follow the procedure below modify the webpage:
- Edit and modify the index.shtml file to fit your needs. Keep in mind that all changes can be reverted thanks to the Git versioning. Tip: Another IDE (e.g. VS Code, Atom, ...) can be used to preview the page while changes are made.
- Execute the makefsdata.exe or use the makefsdata provided by LwIP inside the SDK (location: util/third_party/lwip/lwip/src/apps/http/makefsdata).
- Rename the generated file fsdata.c into httpfsdata.c.
- Edit the file and remove include pragmas except #include "lwip/def.h".
- Rebuild the project and flash the device.
From the SDK Example
The Webpage sources are provided with the SDK example in the lwip_host/fsdata/fs folder.
Follow the procedure below modify the webpage:
- Copy/paste the lwip_host/fsdata/fs folder of your SDK in the same location inside your workspace.
- Edit and modify the index.shtml file to fit your needs. Tip: Another IDE (e.g. VS Code, Atom, ...) can be used to preview the page while changes are made.
- Use the makefsdata provided by LwIP inside the SDK (location: util/third_party/lwip/lwip/src/apps/http/makefsdata) or use the makefsdata.exe (associated with msvcr100d.dll) provided by the GitHub Example (https://github.com/SiliconLabs/wfx-fullMAC-tools/tree/wifi_examples_ssv4/Examples/SiliconLabs/commissioning/webpage) for an easier procedure.
- Rename the generated file fsdata.c into httpfsdata.c.
- Edit the file and remove include pragmas except #include "lwip/def.h".
- Remove the include path $/app/mcu_example/SLSTK3701A_EFM32GG11/micriumos_lwip_wfx/lwip_host/fsdata from the list of the GNU C Language in the Project Properties (Project->Properties->C/C++ General->Paths and Symbols, Includes tab).
- Add the include path pointing to the new httpfsdata.c file, i.e. /$/src/lwip_host/fsdata, and check the box Is a workspace path.
- Rebuild the project and flash the device.
Debugging Tools
GDB
The toolchain provided with Simplicity Studio 4 contains a compiler, a linker, all you need to build a project, and it also contains a debugger. This debugger, called gdb, allows you to walk into the program step by step, to set breakpoints, to access the MCU memory and registers, ... For more information about how to use the debugger inside Simplicity Studio 4, please refer to the section 4. Debugger inside the AN0822: Simplicity Studio™ User's Guide.
Tip: Before starting a debug session, disable the project optimizations by selecting None from the Optimization Level list in the section [Optimization] of [Tools Settings] tab from the Project properties (Project->Properties->C/C++ Build->Settings). By default the project is built using the highest optimization setting to have the highest Wi-Fi performances, making the debug experience painful since the instructions are reorganized, so the program will give the impression not to execute linearly.
Additional Logs
Always with the aim to have the highest possible Wi-Fi performances, only few logs are enabled and they are related to actions happening times to times. Nevertheless, having more logs is often good to track a bug or better understand a program behavior. In that purpose LwIP provides logs in each feature of the stack. These logs are disabled by default but can be enabled by editing the lwipopts.h file of the project. The file purpose is to configure the stack IP, like the features enabled or disabled.
To enable logs related to a specific feature:
- Find the associated define in the feature sources. The define name ends with _DEBUG, like HTTP_DEBUG, MQTT_DEBUG, TCP_DEBUG, ...
- Open the lwipopts.h file located in the lwip_host folder inside the project.
- Enable the global debug define LWIP_DEBUG in the top of the file.
- Enable the feature logs by adding the feature define inside the file and enabling it.
SEGGER SystemView
SEGGER SystemView is a powerful tool allowing to capture all the events (Task switching, Mutex/Semaphore acquisition and release, ...) in a Real-Time Operating System (RTOS) which is particularly helpful to define tasks priorities or to track a behavior leading to a Dead Lock. This tool supports Micrium OS and is provided free of charge with Simplicity Studio, it can be installed from the Simplicity Installation Manager by selecting the [Package Manager] option and the [Tools] tab, then look for the SEGGER SystemView Integration tool and install it. For more information about how to use SEGGER SystemView with Micrium OS, please refer to this documentation.
Optimization Considerations
This section describes steps to increase the throughput while keeping a minimum footprint necessary for your application. The first portion of this document describes the recommended tools. The second portion describes the firmware changes necessary to tweak the performance.
Optimization Tools
iPerf
iPerf is a well_known tool used to measure the throughput on an IP link. This example starts a TCP Server for iPerf testing by default, allowing you to check the throughput after tweaking the program configuration and see the impact. When enabled, the TCP Server for iPerf will be listening for incoming connections at any time. The method to start an iPerf test is dependent on the platform you are using to run the iPerf client:
- For PCs, install iPerf on your machine. Once installed, call the command below:
iperf -c 10.10.0.1
You simply need to issue this command as illustrated in the following image:
- For Android smartphones, install Magic iPerf using the Google Play Store. Open the application and enter the command above without the 'iperf'. Make sure [iPerf2] is selected. You can start the test by using the [Stopped] switch.
- For IOS smartphones, install HE.NET Network Tools using the Apple Store. Open the application and open the side menu to click on 'iperf'. Make sure 'TCP' is selected. Enter the number of bytes you want to send (e.g., 100 M) and finally enter the IP address in the upper text box (e.g., 10.10.0.1). The iPerf test starts.
Micrium OS µC/Probe
Micrium provides the µC/Probe tool free of charge. This tool allows to watch in a graphical manner a program execution, like variables values, statistics, ... A dashboard for this tool is provided with the GitHub example, in the purpose of tracking in run-time the Micrium OS statistics, like the CPU and stack usages. It can also be used on the SDK example by retrieving this file. Note that the tool can also be used with the SDK example by retrieving the dashboard from the GitHub example and copying it inside your project.
To enable the visualization, make sure that the following defines are enabled inside the cfg/os_cfg.h file:
#define OS_CFG_DBG_EN DEF_ENABLED
#define OS_CFG_STAT_TASK_EN DEF_ENABLED
#define OS_CFG_TASK_PROFILE_EN DEF_ENABLED
Optimization Settings
Compiler Optimization
Open the Project’s Compiler Settings and set the Compiler Optimization level to: [Optimize most (-O3)] as shown in the image below. This optimization level will ensure the highest performances associated with a smaller binary.
Micrium OS Configuration
Debugging Configuration
Checks are done inside the Kernel to ensure the action previously done was successful. There can be a lot of checks and if the program behaves without triggering assertions (enabled by default) then it can be considered to disable all (or some of) the Kernel modules to see if it improves the performances. This can be done by editing the configuration file rtos_cfg.h and disabling the API argument check assertions and error logging by setting the following option:
#define RTOS_CFG_ASSERT_DBG_ARG_CHK_EXT_MASK RTOS_CFG_MODULE_NONE
Following the same idea, the Kernel Logs can also be disabled by setting the following option:
#define RTOS_CFG_LOG_EN DEF_DISABLED
The error code extended debugging information can also be disabled inside the configuration file rtos_err_cfg.h by setting the following options:
#define RTOS_ERR_CFG_EXT_EN DEF_DISABLED
#define RTOS_ERR_CFG_STR_EN DEF_DISABLED
Runtime Statistics
Runtime statistics are set by default in the kernel, they can be disabled by editing the configuration file os_cfg.h and disable the kernel runtime statistics as follows:
#define OS_CFG_STAT_TASK EN DEF_DISABLED
#define OS_CFG_TASK_PROFILE_EN DEF_DISABLED
LwIP Configuration
LwIP is an IP stack providing a great granularity to tweak the configuration and reach the best performances. This configuration can be modified by editing the lwipopts.h file located in the lwip_host folder inside the project. The dedicated Maximizing throughput article will help you focus on the main variables to reach the highest performances.
Enabling the LwIP statistics is particularly helpful to dimension the different memory pools. The statistics are enabled as follows in the lwipopts.h file.
#define LWIP_STATS 1
#define LWIP_STATS_DISPLAY 1
This allows to output the statistics in the console by adding a call to the function stats_display() in your application.
Wi-Fi FMAC Driver Documentation
For your own application development or for more information about the Wi-Fi FMAC Driver, please refer to the documentation.
Troubleshooting
Connecting a Silicon Labs Starter Kit associated to a WF(M)200 Expansion Board to your Wireless Network is a complex process. If any of the steps in the process is not done correctly, failure can occur. This section describes a few basic steps you can take to troubleshoot this demo.
Check the Logs from a Serial Terminal
Open a serial terminal as described in the third step of the section Start the Example.
Check the Hardware Connections
Check the boards connection to ensure that the WF(M)200 Expansion Board is inserted tightly into the 20-pin expansion header of the Silicon Labs Starter Kit, as described in section Setup your Kit. Make sure that all the switches are in the correct position, as described in section Setup your Kit.
Verify Wi-Fi Access Point Settings
Use your Wi-Fi router’s (i.e., AP) administrative GUI to verify network settings for the wireless network Service Set Identifier (SSID) to which your WF(M)200 Wi-Fi module is trying to connect. Locate the SSID that you are troubleshooting. On a basic Wi-Fi router, there may be just one SSID, or one for each radio band (2.4 GHz and 5 GHz). If your WF(M)200 and Wi-Fi AP or router can hear each other but still cannot connect or exchange traffic, look for a security mismatch. Configure the Wi-Fi AP or Router to one of the security modes the WF(M)200 supports: Open, WEP, WPA, WPA2 or WPA3 (GitHub Example only).
Verify Network Connection with Ping
If your WF(M)200 still can't connect but you are unable to display the Webpage, check the IP address provided to the WF(M)200. Notice that the WF(M)200 falls back to a default IP address (192.168.0.1) if no IP address is provided by the Wi-Fi AP after a certain time (several tens of seconds). Check that a DHCP server is running on your Wi-Fi router and identify the IP subnet assigned upon a successful connection. Identify the Wi-Fi router’s local IP address that should be reachable through this subnet. Check your Wi-Fi router's events log or status GUI to verify that an IP address from this subnet is assigned to your WF(M)200 when it connects. After your WF(M)200 has a valid IP address, meaning an IP address from the subnet identified earlier, use a ping command from another station or from your Wi-Fi router to verify that your WF(M)200 is connected to the network and is reachable.
Check Wireless-Specific Issues
If your WF(M)200 still can't connect, get a valid IP address or ping your Wi-Fi router. Then, it's time to consider wireless-specific problems. The Wi-Fi AP or router and WF(M)200 must use compatible 802.11 standards and the same network name (SSID). Use your AP or router's admin GUI to view WLAN settings and compare them to your embedded application's wireless connection parameters. Run the scan command in the Serial Console and verify that your Wi-Fi AP or Router is displayed in the list. If your SSID does not appear in the WF(M)200's Available Networks list, enable SSID broadcasts on your AP or router. Be sure to match the SSID exactly, including capitalization.
Check Intermittent Network Connectivity Issues
Finally, if your WF(M)200 connects and pings successfully, but encounters intermittent network connectivity problems (e.g., some pings work, some fail), you may be experiencing poor signal strength, RF interference, or if the demo has been modified, a software-related problem.
If the demo has been modified, such as by adding an additional task or modifying task priorities, see the Micrium OS Kernel Troubleshooting Guide at: https://doc.micrium.com/display/OSUM50700/Kernel+Troubleshooting.