Wi-Fi commissioning demonstration #

For the demo purposes, the WF(M)200 concurrently exposes 2 Wi-Fi interfaces:

The host supports a Web server which exposes a user-accessible Web page. 'Commissioning' means providing the AP 's credentials to the Station over a temporary SoftAP connection from a Wi-Fi Device . This is achieved via the Web page.

At this moment:

  • Your Device is not connected to the SoftAP (it may be connected to another AP )
  • The SoftAP is waiting for a Device to connect
  • The Station is not connected to any AP

Connecting to the SoftAP #

When the SoftAP is started, you can join it with any Wi-Fi Device :

From this Web page you can read and toggle the state of the onboard LEDs. The Device is shown on the left as connected to the SoftAP in the center.

Commissioning #

From the same Web page, you can also connect the Station to a Wi-Fi Access Point (the AP ) as follows:

The kit has been commissioned successfully .

At this moment:

  • The Station is connected to the AP
  • Your Device is still connected to the SoftAP

Indirect Communication with the Kit #

At this moment:

  • The Station is connected to the AP
  • Your Device is not connected to the SoftAP anymore
  • Your Device is indirectly connected to the kit via the AP