API constant valuesFULL_MAC_API

WFM API constant values.

Macros

#define SL_WFX_FMAC_MAC_ADDR_SIZE SL_WFX_MAC_ADDR_SIZE
Length of the MAC address element.
#define SL_WFX_FMAC_BSSID_SIZE SL_WFX_BSSID_SIZE
Length of the BSSID element.
#define SL_WFX_PASSWORD_SIZE 64
Length of the password element.
#define SL_WFX_CHANNEL_NUMBER_SIZE 14
Maximum length of the channel list element.
#define SL_WFX_SSID_DEF_SIZE 2
Maximum length of the SSID list element.
#define SL_WFX_FMAC_SSID_SIZE SL_WFX_SSID_SIZE
Length of the Service Set Identifier (SSID) element.
#define SL_WFX_ARP_IP_ADDR_SIZE 2
Length of the ARP IP address list element.
#define SL_WFX_NS_IP_ADDR_SIZE 2
Length of the NS IP address list element.
#define SL_WFX_IPV6_ADDR_SIZE 16
Length of the IPv6 address element.

Enumerations

enum sl_wfx_client_isolation_t {
WFM_CLIENT_ISOLATION_DISABLED = 0x0,
WFM_CLIENT_ISOLATION_ENABLED = 0x1
}
Client Isolation toggling.
enum sl_wfx_frame_type_t {
WFM_FRAME_TYPE_MGMT = 0x0,
WFM_FRAME_TYPE_ACTION = 0x4,
WFM_FRAME_TYPE_DATA = 0x8
}
Type of frame to be sent.
enum sl_wfx_hidden_ssid_t {
WFM_HIDDEN_SSID_FALSE = 0x0,
WFM_HIDDEN_SSID_TRUE = 0x1
}
Hidden SSID toggling.
enum sl_wfx_mgmt_frame_protection_t {
WFM_MGMT_FRAME_PROTECTION_DISABLED = 0x0,
WFM_MGMT_FRAME_PROTECTION_OPTIONAL = 0x1,
WFM_MGMT_FRAME_PROTECTION_MANDATORY = 0x2
}
Device Protected Management Frame mode.
enum sl_wfx_pm_mode_t {
WFM_PM_MODE_ACTIVE = 0x0,
WFM_PM_MODE_PS = 0x1,
WFM_PM_MODE_DTIM = 0x2
}
Device power management mode.
enum sl_wfx_priority_t {
WFM_PRIORITY_BE0 = 0x0,
WFM_PRIORITY_BK1 = 0x1,
WFM_PRIORITY_BK2 = 0x2,
WFM_PRIORITY_BE3 = 0x3,
WFM_PRIORITY_VI4 = 0x4,
WFM_PRIORITY_VI5 = 0x5,
WFM_PRIORITY_VO6 = 0x6,
WFM_PRIORITY_VO7 = 0x7
}
Data priority level per 802.1D.
enum sl_wfx_reason_t {
WFM_REASON_UNSPECIFIED = 0x0,
WFM_REASON_TIMEOUT = 0x1,
WFM_REASON_LEAVING_BSS = 0x2,
WFM_REASON_UNKNOWN_STA = 0x3,
WFM_REASON_AP_FULL = 0x4,
WFM_REASON_AUTHENTICATION_FAILURE = 0x5
}
Reasons for AP to reject or disconnect a client.
enum sl_wfx_disconnected_reason_t {
WFM_DISCONNECTED_REASON_UNSPECIFIED = 0x0,
WFM_DISCONNECTED_REASON_AP_LOST = 0x1,
WFM_DISCONNECTED_REASON_REJECTED = 0x2,
WFM_DISCONNECTED_REASON_LEAVING_BSS = 0x3,
WFM_DISCONNECTED_REASON_WPA_COUNTERMEASURES = 0x4
}
Reasons for STA disconnection.
enum sl_wfx_scan_mode_t {
WFM_SCAN_MODE_PASSIVE = 0x0,
WFM_SCAN_MODE_ACTIVE = 0x1
}
Scan mode to be used.
enum sl_wfx_security_mode_t {
WFM_SECURITY_MODE_OPEN = 0x0,
WFM_SECURITY_MODE_WEP = 0x1,
WFM_SECURITY_MODE_WPA2_WPA1_PSK = 0x2,
WFM_SECURITY_MODE_WPA2_PSK = 0x4,
WFM_SECURITY_MODE_WPA3_SAE = 0x6
}
Security mode of a network.
enum sl_wfx_ext_auth_data_type_t
Type of the authentication message.
enum sl_wfx_fmac_status_t {
WFM_STATUS_SUCCESS = 0x0,
WFM_STATUS_INVALID_PARAMETER = 0x1,
WFM_STATUS_WRONG_STATE = 0x2,
WFM_STATUS_GENERAL_FAILURE = 0x3,
WFM_STATUS_CHANNEL_NOT_ALLOWED = 0x4,
WFM_STATUS_WARNING = 0x5,
WFM_STATUS_NO_MATCHING_AP = 0x6,
WFM_STATUS_CONNECTION_ABORTED = 0x7,
WFM_STATUS_CONNECTION_TIMEOUT = 0x8,
WFM_STATUS_CONNECTION_REJECTED_BY_AP = 0x9,
WFM_STATUS_CONNECTION_AUTH_FAILURE = 0xA,
WFM_STATUS_RETRY_EXCEEDED = 0x13,
WFM_STATUS_TX_LIFETIME_EXCEEDED = 0x14,
WFM_STATUS_REQUEUE = 0x15
}
Full MAC (UMAC) confirmation possible values for a returned 'status' field.

Detailed Description

WFM API constant values.

Macro Definition Documentation

◆ SL_WFX_ARP_IP_ADDR_SIZE

#define SL_WFX_ARP_IP_ADDR_SIZE   2

Length of the ARP IP address list element.

Definition at line 220 of file sl_wfx_cmd_api.h .

◆ SL_WFX_CHANNEL_NUMBER_SIZE

#define SL_WFX_CHANNEL_NUMBER_SIZE   14

Maximum length of the channel list element.

Definition at line 214 of file sl_wfx_cmd_api.h .

◆ SL_WFX_FMAC_BSSID_SIZE

#define SL_WFX_FMAC_BSSID_SIZE   SL_WFX_BSSID_SIZE

Length of the BSSID element.

Definition at line 210 of file sl_wfx_cmd_api.h .

◆ SL_WFX_FMAC_MAC_ADDR_SIZE

#define SL_WFX_FMAC_MAC_ADDR_SIZE   SL_WFX_MAC_ADDR_SIZE

Length of the MAC address element.

Definition at line 208 of file sl_wfx_cmd_api.h .

◆ SL_WFX_FMAC_SSID_SIZE

#define SL_WFX_FMAC_SSID_SIZE   SL_WFX_SSID_SIZE

Length of the Service Set Identifier (SSID) element.

Definition at line 218 of file sl_wfx_cmd_api.h .

◆ SL_WFX_IPV6_ADDR_SIZE

#define SL_WFX_IPV6_ADDR_SIZE   16

Length of the IPv6 address element.

Definition at line 224 of file sl_wfx_cmd_api.h .

◆ SL_WFX_NS_IP_ADDR_SIZE

#define SL_WFX_NS_IP_ADDR_SIZE   2

Length of the NS IP address list element.

Definition at line 222 of file sl_wfx_cmd_api.h .

◆ SL_WFX_PASSWORD_SIZE

#define SL_WFX_PASSWORD_SIZE   64

Length of the password element.

Definition at line 212 of file sl_wfx_cmd_api.h .

Referenced by sl_wfx_get_pmk() .

◆ SL_WFX_SSID_DEF_SIZE

#define SL_WFX_SSID_DEF_SIZE   2

Maximum length of the SSID list element.

Definition at line 216 of file sl_wfx_cmd_api.h .

Enumeration Type Documentation

◆ sl_wfx_client_isolation_t

Client Isolation toggling.

Enumerator
WFM_CLIENT_ISOLATION_DISABLED

Client isolation disabled.

WFM_CLIENT_ISOLATION_ENABLED

Client isolation enabled.

Definition at line 229 of file sl_wfx_cmd_api.h .

◆ sl_wfx_disconnected_reason_t

Reasons for STA disconnection.

Enumerator
WFM_DISCONNECTED_REASON_UNSPECIFIED

Unspecified reason.

WFM_DISCONNECTED_REASON_AP_LOST

AP timed out.

WFM_DISCONNECTED_REASON_REJECTED

Disconnected by AP.

WFM_DISCONNECTED_REASON_LEAVING_BSS

Leaving intentionally.

WFM_DISCONNECTED_REASON_WPA_COUNTERMEASURES

WPA countermeasures triggered a disconnection.

Definition at line 301 of file sl_wfx_cmd_api.h .

◆ sl_wfx_fmac_status_t

Full MAC (UMAC) confirmation possible values for a returned 'status' field.

All Full MAC (UMAC) confirmation messages have a field 'status' just after the message header.
A value of zero indicates the request has completed successfully.

Enumerator
WFM_STATUS_SUCCESS

The device has successfully completed a request.

WFM_STATUS_INVALID_PARAMETER

A request contains one or more invalid parameters.

WFM_STATUS_WRONG_STATE

The request cannot be performed because the device is in an inappropriate state.

WFM_STATUS_GENERAL_FAILURE

The request failed due to an error.

WFM_STATUS_CHANNEL_NOT_ALLOWED

The request failed due to regulatory limitations.

WFM_STATUS_WARNING

The request is successful but some parameters have been ignored.

WFM_STATUS_NO_MATCHING_AP

The request failed because no suitable AP was found for the connection.

WFM_STATUS_CONNECTION_ABORTED

The request failed because the user issued a WFM_HI_DISCONNECT_REQ before completing the connection.

WFM_STATUS_CONNECTION_TIMEOUT

The request failed because a timeout occurred during connection.

WFM_STATUS_CONNECTION_REJECTED_BY_AP

The request failed because the AP rejected the connection.

WFM_STATUS_CONNECTION_AUTH_FAILURE

The request failed because the WPA handshake did not complete successfully.

WFM_STATUS_RETRY_EXCEEDED

The request failed because the retry limit was exceeded.

WFM_STATUS_TX_LIFETIME_EXCEEDED

The request failed because the MSDU life time was exceeded.

WFM_STATUS_REQUEUE

The request failed because TX is suspended (temperature too high)

Definition at line 344 of file sl_wfx_cmd_api.h .

◆ sl_wfx_frame_type_t

Type of frame to be sent.

Value unused, all frames are considered to be Data by default.
Support for the other types will be added later.

Enumerator
WFM_FRAME_TYPE_MGMT

Management Frame.

WFM_FRAME_TYPE_ACTION

Action Frame.

WFM_FRAME_TYPE_DATA

Data Frame.

Definition at line 240 of file sl_wfx_cmd_api.h .

◆ sl_wfx_hidden_ssid_t

Hidden SSID toggling.

Enumerator
WFM_HIDDEN_SSID_FALSE

SSID not hidden.

WFM_HIDDEN_SSID_TRUE

SSID hidden.

Definition at line 249 of file sl_wfx_cmd_api.h .

◆ sl_wfx_mgmt_frame_protection_t

Device Protected Management Frame mode.

Enumerator
WFM_MGMT_FRAME_PROTECTION_DISABLED

PMF disabled.

WFM_MGMT_FRAME_PROTECTION_OPTIONAL

PMF optional.

WFM_MGMT_FRAME_PROTECTION_MANDATORY

PMF mandatory.

Definition at line 257 of file sl_wfx_cmd_api.h .

◆ sl_wfx_pm_mode_t

Device power management mode.

Enumerator
WFM_PM_MODE_ACTIVE

Always on.

WFM_PM_MODE_PS

Use power_save and wake up on beacons.

WFM_PM_MODE_DTIM

Use power_save and wake up on DTIM.

Definition at line 266 of file sl_wfx_cmd_api.h .

◆ sl_wfx_priority_t

Data priority level per 802.1D.

Enumerator
WFM_PRIORITY_BE0

Best Effort.

WFM_PRIORITY_BK1

Background.

WFM_PRIORITY_BK2

Background.

WFM_PRIORITY_BE3

Best Effort.

WFM_PRIORITY_VI4

Video.

WFM_PRIORITY_VI5

Video.

WFM_PRIORITY_VO6

Voice.

WFM_PRIORITY_VO7

Voice.

Definition at line 275 of file sl_wfx_cmd_api.h .

◆ sl_wfx_reason_t

Reasons for AP to reject or disconnect a client.

Enumerator
WFM_REASON_UNSPECIFIED

Unspecified reason (unused)

WFM_REASON_TIMEOUT

Client timed out.

WFM_REASON_LEAVING_BSS

Client left.

WFM_REASON_UNKNOWN_STA

Client not authenticated.

WFM_REASON_AP_FULL

Too many clients already connected.

WFM_REASON_AUTHENTICATION_FAILURE

WPA authentication failed.

Definition at line 289 of file sl_wfx_cmd_api.h .

◆ sl_wfx_scan_mode_t

Scan mode to be used.

Enumerator
WFM_SCAN_MODE_PASSIVE

Passive scan: listen for beacons only.

WFM_SCAN_MODE_ACTIVE

Active scan: send probe requests.

Definition at line 312 of file sl_wfx_cmd_api.h .

◆ sl_wfx_security_mode_t

Security mode of a network.

Enumerator
WFM_SECURITY_MODE_OPEN

No security.

WFM_SECURITY_MODE_WEP

Use WEP.

WFM_SECURITY_MODE_WPA2_WPA1_PSK

Use WPA1 or WPA2.

WFM_SECURITY_MODE_WPA2_PSK

Use only WPA2.

WFM_SECURITY_MODE_WPA3_SAE

Use WPA3 (STA mode only)

Definition at line 320 of file sl_wfx_cmd_api.h .